15300027 by Aptiv PLC

Overview of 15300027 by Aptiv PLC

The 15300027 is a Combination Line Connector characterized by a 2-contact configuration, tailored for female crimp terminal connections. This automotive housing component is a 2-position, black, sealed female connector assembly, belonging to the Metri-Pack 280 Series. Notably, this part is designed to be compatible with several specific cables, improving its utility in various connecting environments. Made from polyamide 66, it ensures durability and resistance to environmental factors. This part is a general-purpose component meant primarily for cable mounting and utilizes a crimp termination type.

Industry Applications for 15300027

The 15300027 could serve multiple industry applications due to its robust design and specifications. Here are a few potential industry use cases:

  • Automotive: This connector could potentially be used in automotive applications, especially because it is designed as an automotive housing component. For instance, it might connect various sensors or actuators in a vehicle’s electrical system.
  • Consumer Electronics: Devices that require reliable connection systems such as home automation systems or high-end audiovisual equipment could benefit from the robustness of this connector.
  • Industrial Automation: In industrial settings, the reliability and specification of the 15300027 could make it suitable for connecting machinery or automation components that require precise and secure connections.
  • Telecommunications: The connector could be used in network hardware setups like routers or switches where secure connections are essential for consistent performance and reliability.
  • Electronic Manufacturing: This connector might be utilized in the manufacturing process of various electronic devices, aiding in the assembly of complex electronic systems.

Note that these potential industry applications are conceptual and require verification for compliance with specific standards and suitability for the intended use.

About Aptiv PLC

Aptiv PLC, the manufacturer of the 15300027, is a recognized global technology company that focuses on the design and manufacture of electrical and electronic solutions needed for a safer, greener, and more connected future. In the Combination Line Connectors market, Aptiv stands out by producing high-quality, reliable parts that cater to a broad range of applications across various industries. This specific connector represents one of its versatile solutions that align with modern connectivity demands.

Where to Find 15300027 by Aptiv PLC

To find the 15300027 for purchase, you can research on findchips.com. By navigating to the Combination Line Connectors section, you can also explore alternate parts offered by Aptiv PLC or other manufacturers. Historically, this part has been available through various distributors such as Master Electronics, Bristol Electronics, TTI, Quest Components, and Mouser Electronics. However, current availability, stock levels, and pricing can be best verified directly through FindChips.

Compare pricing for 15300027 and other Combination Line Connectors / Connectors at findchips.com