172166-1 by TE Connectivity

Overview of 172166-1 by TE Connectivity

The 172166-1 by TE Connectivity is a connector housing plug defined by its 3-way connection capability, with a mating pitch of 4.14mm, designed primarily for cable mount applications. This component, composed of Nylon (Polyamide66), underscores its utility in an array safer and controlled environments where the integrity of the connection is paramount. As part of the Combination Line Connectors subcategory, this part offers versatility for various electrical circuits by accommodating 3 rectangular power connectors within a plug body style. Its physical dimensions, including a body breadth of 0.22 inches, depth of 0.933 inches, and length of 0.591 inches, make it a compact solution for applications where space and reliability are considerations. Moreover, its compliance with ROHS and being lead-free indicate its suitability for modern environmentally conscious electronic designs. Additionally, characterized by a natural insulator color, it supports operating temperatures ranging from -20 °C to 105 °C and has a rated voltage of 600 V, making it dynamic across various operating conditions.

Industry Applications for 172166-1

The 172166-1 connector, with its Nylon housing and capability to work within a wide range of temperatures, has potential applications across multiple industries. Below are a few examples where this component could find use, though it’s important to note that these applications are conceptual and should be verified by engineering teams:

  • Consumer Electronics: In devices requiring reliable power connections with low to moderate power requirements, such as handheld gadgets or home appliances.
  • Environmental Monitoring Systems: This plug could be used in sensors and devices designed for tracking environmental conditions, where its insulation resistance and durability would be beneficial.
  • Agriculture Technology: Modern farming equipment and sensors that monitor crop and soil conditions could leverage the 172166-1 for its reliable electrical connections.
  • Internet of Things (IoT) and Smart Cities: In IoT devices and infrastructure components used in smart city initiatives, where compact, dependable connectivity solutions are critical.
  • Medical Imaging and Healthcare: Equipment like non-invasive scanners that require stable connections might utilize the 172166-1, assuming it meets all specific safety and reliability standards for medical devices.
  • Robotics and Drones: These applications benefit from the connector’s durability, capable of maintaining connections despite the vibrations and movements typical in such dynamic applications.

These potential applications illustrate the versatility of the 172166-1 connector, reflecting its design and material properties which support a broad array of use cases across industries.

About TE Connectivity

TE Connectivity is a global leader in connectivity and sensor solutions, known for its innovation and excellence in engineering across a variety of industries. In the realm of Combination Line Connectors and connectors at large, TE Connectivity prides itself on offering a diverse portfolio of products that meet the rigorous requirements of industrial, commercial, and residential applications. The 172166-1 represents just one example of TE Connectivity’s approach to designing and manufacturing connectors that facilitate reliable and efficient electrical connections. TE Connectivity leverages advanced materials, extensive industry expertise, and a commitment to sustainability to ensure its products, including the 172166-1 and similar parts, are at the forefront of technology and meet the evolving needs of modern electronic designs.

Where to Find 172166-1 by TE Connectivity

To source the 172166-1, it’s recommended to search on findchips.com for the most current stock levels and competitive pricing across a wide range of distributors. For sourcing Combination Line Connectors, findchips.com remains an invaluable tool in finding not only the 172166-1 but also alternate parts that might be suited for your application, offered by TE Connectivity or other manufacturers. Traditional distributors of the 172166-1 have included New Advantage Corporation, Master Electronics, and LCSC, among others such as DigiKey and Mouser Electronics. However, availability can fluctuate, and it’s important to consult findchips.com for the latest information regarding distributors and stock levels.

Compare pricing for 172166-1 and other Combination Line Connectors / Connectors at findchips.com