Overview of 350180 by TE Connectivity
The 350180 by TE Connectivity is a test probe assembly specifically designed for use with printed circuit boards (PCBs). This component is integral to ensuring the functionality and integrity of PCBs by facilitating testing and signal checking. The assembly includes a banana jack connector which utilizes a solder-type termination, ensuring a reliable and secure connection to the PCB. The body of the connector is made from brass, with an insulator color of black, which matches its overall black aesthetic. Additionally, the part is RoHS compliant, adhering to stringent environmental and safety standards regarding the restriction of hazardous substances.
This part falls within the subcategory of Other Interconnects under the category of Connectors, highlighting its role in facilitating interconnections in various electronic assemblies. The connector is denoted as an interconnection device with a mounting type specified as board, indicating its application on PCBs. Pertinent technical specifications include a mounting hole diameter of 1.372mm and a rated current of 4.75A for signal applications, providing robust performance for a wide range of applications. The factory lead time for this part is approximately 13 weeks and 3 days, as of the current writing.
Industry Applications for 350180
The 350180, with its specifications and capabilities, could potentially be utilized across a diverse range of industry applications. These fields leverage electronic connections prominently, particularly in sensitive or critical electronics environments. Note that these potential applications are highly conceptual and should be rigorously vetted by engineering and design teams according to specific requirements:
- Consumer Electronics: Devices such as smartphones, laptops, and other personal electronics could possibly incorporate this test probe during the manufacturing and testing phase to ensure quality and performance. The solder type termination and reliable brass body may be significant in environments requiring durability and precision.
- Telecommunications: In telecom equipment, precise and reliable interconnection is crucial. The 350180 could potentially be used in the testing phases of development for routers, switches, and related infrastructure to ensure reliable service delivery.
- Computing and Data Storage: Given the critical nature of reliable data management, components used in servers and storage devices must be thoroughly tested. The 350180, with its specific design for PCBs, may be used to verify the integrity and performance of these systems.
- Automotive: In scenarios where the automotive industry contains electronics requiring rigorous testing for safety and performance, such as in vehicle control systems, the 350180 could potentially play a role during the prototyping and development stages.
It is important to note that selecting the 350180 for these applications requires thorough analysis and verification by professionals to ensure compliance with industry specifications and performance requirements.
About TE Connectivity
TE Connectivity is a global technology leader in connectivity and sensor solutions that are essential in today’s increasingly connected world. TE Connectivity designs and manufactures products at the heart of electronic connections for the world’s leading industries including automotive, industrial equipment, data communication systems, aerospace, defense, medical, oil and gas, consumer electronics and energy.
Specific to the realm of Other Interconnects, TE Connectivity provides a broad range of connector types including the 350180, designed for various applications across multiple sectors. The company excels in crafting high-precision parts that accommodate intricate electronic assemblies, helping to advance innovations in connectivity and enhance the performance and reliability of electronic systems.
Where to Find 350180 by TE Connectivity
To purchase the 350180, it is advisable to visit findchips.com where you can check current stock levels, obtain pricing information, and view offerings from multiple distributors. Historically, this part has been available from distributors such as Neutron USA, Master Electronics, Powell Electronics, and Mouser Electronics. Availability and pricing can fluctuate, so visiting findchips.com will provide the most current information.
For those looking for alternate parts similar to 350180 or other offerings by TE Connectivity and different manufacturers in the Other Interconnects subcategory, findchips.com also maintains a comprehensive listing that could aid in comparison and selection based on specific project requirements.