453-00039R by Laird, A DuPont Business

Overview of 453-00039R by Laird, A DuPont Business

The 453-00039R is categorized as a Bluetooth Module 5.1 featuring 1Mbps, 2Mbps, and 125kbps speed options, with an integrated antenna for transmit and receive operations, suited to smd (surface-mount device) assembly. This part falls under the Other Telecom ICs subcategory of Telecommunications Circuits. The module is designed to comply with the 802.15.4 standard for PAN (Personal Area Network) such as Bluetooth technologies, crucial for applications requiring wireless connectivity.

RoHS compliant, indicated by the RoHS Code “Yes,” implies that the 453-00039R adheres to the restrictions on the use of certain hazardous substances in electrical and electronic equipment. Its part life cycle code “Transferred” suggests that it is either at or has been moved to a mature stage in its product life cycle. The peak reflow temperature of 260°C and maximum duration of the reflow time at peak temperature are critical for manufacturers to understand as they relate to the soldering process in PCB assembly. With a described factory lead time of 16 weeks, planning for procurement requires foresight, particularly during design and production scaling stages.

Industry Applications for 453-00039R

The broad capabilities of the 453-00039R make it suitable for a range of industry applications, where its integration can foster enhanced connectivity and control. Here, we explore potential applications though it must be noted that these uses should be verified by engineering and design teams based on specific requirements:

  • Consumer Electronics: Devices like smart watches, fitness trackers, and wireless headsets could potentially incorporate this module to manage Bluetooth connectivity, offering seamless communication between devices.
  • Healthcare: Medical devices that require low-energy and reliable connectivity for data transmission such as patient monitoring systems might use this Bluetooth module. Integration of such technology in healthcare devices facilitates real-time data collection and health monitoring.
  • Smart Cities: In the scope of smart infrastructure, components like the 453-00039R could be integrated into traffic control systems or public transport to relay real-time information and enhance connectivity between various city services.
  • Automated Industrial Systems: In industrial environments, wireless modules can facilitate the communication between sensors and control systems, potentially improving efficiency of operations and system diagnostics.
  • Wearable Technology: Augmented reality glasses and similar wearable tech could leverage 453-00039R for their Bluetooth capabilities, enabling these devices to communicate with smartphones or other connected devices.

These potential industry applications are conceptual and should undergo rigorous testing and validation according to industry standards and specific application requirements.

About Laird, A DuPont Business

Laird, A DuPont Business, plays a significant role in the telecommunications industry, specializing in advanced technology solutions like the 453-00039R. Their expertise spans a variety of components that facilitate reliable and efficient telecommunications across multiple platforms. Laird produces not only Bluetooth modules but also a range of RF solutions that address the needs of modern wireless communications systems. Their products typically feature robust performance specifications suited to demanding telecommunication applications, illustrating their commitment to innovation and quality in this field.

Where to Find 453-00039R by Laird, A DuPont Business

To source the 453-00039R, potential buyers should consult FindChips.com for the most up-to-date availability data. While this part has previously been available through distributors such as Symmetry Electronics, Avnet Asia, Mouser Electronics, Avnet Americas, and DigiKey, inventory levels can fluctuate. Interested parties are advised to check current stock levels and pricing directly from these or alternative suppliers on FindChips.com. Additionally, for alternative options and comparable products within the Other Telecom ICs category, one can explore a wide range of similar parts offered by Laird and other manufacturers.

Compare pricing for 453-00039R and other Other Telecom ICs / Telecommunication Circuits at findchips.com