690-004-660-023 by EDAC Inc

Overview of 690-004-660-023 by EDAC Inc.

The 690-004-660-023 is a Telecom and Datacom connector specifically designed for applications requiring USB connectivity. This component features four contacts and has a female straight configuration with solder terminals. It is RoHS compliant, indicating that it adheres to the restriction of hazardous substances in electrical and electronic equipment. Its construction details include a USB 3.0 Type B receptacle, which allows for efficient data transmission. The connector is classified as suitable for general-purpose use, as indicated by its option designation.

Technical attributes include a contact resistance of 30 mΩ, dielectric withstanding voltage rated at 707 VAC, and an impressive insulation resistance of 1 GΩ. The component is manufactured by EDAC Inc., a known entity in the industry, especially in the realm of connectors. Its active part life cycle ensures that it is currently produced and available for procurement. The part also features a mounting option that includes locking capabilities, which can enhance the stability of connections in various applications.

Industry Applications for 690-004-660-023

This electronic component may find potential applications across a variety of industries where reliable USB connections are required. Below are several potential use cases:

  • Industrial Automation: The 690-004-660-023 could serve as a connection point within industrial machinery that utilizes USB interfaces for programming or data transfer. Its solder terminal configuration and robust design may potentially make it suitable for environments where durability is crucial.
  • Internet of Things (IoT): In IoT devices, reliable and efficient data communication is pivotal. As the part supports USB connectivity, it might be utilized in various IoT applications such as smart sensors and devices, facilitating data transfer and power supply.
  • Consumer Electronics: The 690-004-660-023 might also have applications within consumer electronics, possibly in devices like printers or external hard drives, where USB Type B connectors are standard for data communication and device interaction.
  • Medical Imaging: Given its ROSH compliance, the part may find potential use in medical imaging devices that require USB interfaces for connectivity without the risk of hazardous materials affecting performance or safety.
  • Smart Cities: In infrastructure related to smart cities, this component might be employed in data transmission systems that connect various devices, supporting enhanced data flow and communication among different systems.

It is important to note that these potential industry applications for the 690-004-660-023 are conceptual and illustrative. Any specific application should undergo thorough analysis and validation by engineering and design teams to ensure adherence to relevant industry standards and specific requirements.

About EDAC Inc.

EDAC Inc. is a recognized manufacturer specializing in various types of connectors, particularly within the realm of Telecom and Datacom Connectors. The company has a broad portfolio that includes a variety of connection solutions to cater to the evolving demands of multiple industries. The 690-004-660-023 connector is just one of many products aimed at enhancing communication and data transfer. EDAC’s commitment to quality is evidenced through compliance with standards such as RoHS and its proactive approach to producing active components like this USB connector. Similar parts made by EDAC may include various configurations of USB connectors and other types of Telecom connectors that facilitate connectivity in different applications.

Where to Find 690-004-660-023 by EDAC Inc.

690-004-660-023, it is advisable to visit findchips.com, a resourceful platform offering insights into stock levels, pricing, and availability. The part belongs to the category of Telecom and Datacom Connectors, where you might find alternate options either from EDAC Inc. or other manufacturers.

Historically, the part has been available from distributors such as:

  • New Advantage Corporation
  • Master Electronics
  • Bristol Electronics
  • Quest Components
  • Future Electronics
  • DigiKey
  • Mouser Electronics

However, it is recommended to check findchips.com for the most current stock levels and pricing before making any purchasing decisions.

Compare pricing for 690-004-660-023 and other Telecom and Datacom Connectors / Connectors at findchips.com