Overview of 745254-6 by TE Connectivity
The TE Connectivity 745254-6 is a high-quality, durable D-Sub contact designed for crimping onto 26-22 AWG wire. These pin contacts are made from brass with gold-plated contacts to ensure excellent electrical conductivity and resistance to corrosion. They are specifically designed for use with TE Connectivity’s Amplimite HDP-20 Series and CPC D-Sub connectors. The gold plating on the contacts provides a reliable connection with superior performance for signal transmission. This part is RoHS compliant, making it suitable for use in various applications where environmental considerations are important.
Industry Applications for 745254-6
The extensive applications of the 745254-6 D-Sub contact pin across various industries are due to its robust design, connectivity reliability, and the trust in the manufacturer, TE Connectivity. Here are some potential industry applications, keeping in mind that these are conceptual and should be further analyzed by engineering and design teams:
- Space Technology: One could use these contacts in the assembly of satellites or space vehicle electronics because of their reliable electrical performance and resistance to harsh environments.
- Aerospace and Defense: In applications such as avionics systems, these D-Sub contacts might be utilized for their durability and resistance to temperature variations.
- Transportation and Logistics: They may find use in railway signaling systems or in the connectivity solutions of electric vehicle charging stations, owing to their rated current capacity and operating temperature range.
- Renewable Energy: In solar panel installations or wind turbines, these contacts could be used within control systems, providing a reliable connection in environmentally challenging conditions.
- Robotics and Drones: Given their small size, reliability, and the preciseness of connection, these contacts might be ideal for use in the intricate electronics of robots or drones.
Note that the mentioned potential applications require thoughtful consideration and validation by professional engineers to ensure compatibility and performance requirements are met.
About TE Connectivity
TE Connectivity, the manufacturer of 745254-6, is a global technology leader, known for its expertise in engineering advanced connectivity and sensor solutions that are critical in today’s increasingly connected world. TE Connectivity specializes in various domains, including but not limited to Assembly Items of Connector Support. The company focuses on designing and manufacturing highly reliable and precision-engineered components, such as the 745254-6 D-Sub contacts, that find applications in an array of industries from automotive to aerospace, energy, broadband communications, consumer electronics, healthcare, and industrial equipment.
Where to Find 745254-6 by TE Connectivity
For those looking to purchase the TE Connectivity 745254-6, the first point of reference should be findchips.com. The site provides up-to-date information on stock availability, pricing from various distributors, and detailed part data attributes. To explore alternatives or similar parts offered by TE Connectivity or other manufacturers, one can browse the Assembly Items category. Historically, this part has been available at distributors such as Master Electronics, Chip 1 Exchange, Sager, Powell Electronics, and Mouser Electronics. However, it is crucial to verify current stock levels and pricing directly on findchips.com due to the dynamic nature of component availability and market pricing.