453-00045C by Laird, A DuPont Business

Overview of 453-00045C by Laird, A DuPont Business

The 453-00045C module by Laird, A DuPont Business, serves as a Wireless RF with Chip Antenna incorporating Bluetooth and Wi-Fi v5.0/802.11ac technologies. This dual-band module operates on 3.3V and covers both 2.4GHz and 5GHz frequencies. Designed primarily for embedding into modern electronic devices, the module comes in an SMD (Surface-Mount Device) format and is provided on tape, though not on a reel. Its design facilitates integration into various electronic assemblies, ensuring robust and reliable wireless communication capabilities.

This product adheres to the latest industrial standards for environmental safety, as indicated by its RoHS compliance, and is classified under the transferred life cycle phase in Laird’s product catalog. The module’s peak reflow temperature can reach up to 250°C with a maximum time at peak temperature of 50 seconds, illustrating its compatibility with standard PCB assembly processes. Notably, this part is part of the Network Interfaces subcategory in the broader realm of Telecommunication Circuits. As of the current writing, 453-00045C’s factory lead time stands at 26 weeks, which might influence procurement strategies.

Industry Applications for 453-00045C

This component is versatile enough to potentially serve various technological sectors:

  • Education and Research: The 453-00045C could potentially be employed in educational tools and research equipment that require wireless data transmission and connectivity, such as remote sensors or interactive learning devices. Its dual-band capability improves the reliability and speed of connections, which are crucial in research environments where data integrity is paramount.
  • Consumer Electronics: In consumer electronics, this module might be integrated into products like smart home devices, wearable technology, or personal electronics where seamless and efficient Bluetooth and Wi-Fi connectivity are essential. The component’s small form factor and dual-band support make it suitable for compact devices that require robust wireless functionality.
  • Audio and Video Systems: Another potential application might be in audio and video systems like wireless speakers, headphones, or streaming devices. The 453-00045C can facilitate high-quality audio streaming and smooth video playback over Wi-Fi, enhancing user experience.

These potential industry applications are purely illustrative and require detailed analysis and verification by engineering and design teams to ensure compliance with industry standards and specific application needs.

About Laird, A DuPont Business

Laird, A DuPont Business, is known for its substantial contributions to the field of Telecommunication Circuits, particularly in the area of Network Interfaces. Products like the 453-00045C reflect the company’s commitment to providing advanced connectivity solutions. This dedication is evident in their broad array of components that cater to a diverse range of data transmission needs within various applications. By integrating advanced technologies such as Bluetooth and Wi-Fi into compact and efficient modules, Laird continues to support and drive innovations across multiple sectors.

Where to Find 453-00045C by Laird, A DuPont Business

For those interested in acquiring the 453-00045C, it is advisable to start your search at findchips.com. By consulting this platform, you can access current stock levels, pricing, and available distributors. Historically, the part has been available through distributors such as Symmetry Electronics, Avnet Asia, GLYN GmbH & Co. KG, Mouser Electronics, Avnet Americas, and DigiKey. However, availability can fluctuate, and consulting findchips.com will provide up-to-date information. Additionally, by visiting the Network Interfaces section, one can view alternative components that might also meet specific requirements, potentially offered by Laird or other manufacturers.

Compare pricing for 453-00045C and other Network Interfaces / Telecommunication Circuits at findchips.com