Overview of BFR93AE6327HTSA1 by Infineon Technologies AG
The BFR93AE6327HTSA1 from Infineon Technologies AG is a NPN silicon RF Small Signal Bipolar Transistor designed for high-frequency amplification. This device is characterized by its robust handling of power with a maximum power dissipation of 300mW and a continuous collector current of 90mA. It operates under a maximum collector-emitter voltage of 12V and supports a transition frequency up to 6GHz, making it suitable for high-speed switching and RF amplification applications.
Moreover, this transistor is housed in a small outline, R-PDSO-G3 package, which is practical for various high-density mounting requirements. The package supports a gull wing terminal form, enhancing its applicability in surface mount technology. Engineered for high temperature operations, this transistor can function at temperatures up to 150°C. The part is also RoHS compliant and supports Pb-free soldering, aligning with modern environmental and health standards.
As of the current writing, the factory lead time for this part is 16 weeks and 3 days, which is vital for planning and procurement strategies in production schedules.
Industry Applications for BFR93AE6327HTSA1
The BFR93AE6327HTSA1 has potential uses in various industries due to its high frequency and power handling capabilities. However, it is crucial to note that the suggested applications are conceptual and should be verified by engineering teams to meet specific standards and requirements.
- Telecommunications: The transistor could potentially be used in RF amplification circuits within cellular base stations or in RF transceivers. Its ability to operate at 6GHz transition frequency supports applications in high-speed communication systems.
- Audio and Video Systems: In audio processing equipment, this component might play a role in signal amplification to ensure high-quality output. Its high power dissipation capability can be crucial in preventing signal loss over longer audio transmission paths.
- Entertainment and Gaming: Used possibly in wireless communication devices or advanced gaming consoles that require rapid signal processing and output. The high transition frequency supports enhanced gameplay experiences through better handling of RF signals.
It should be reiterated that these potential uses require thorough validation to ensure compatibility and reliability in specific applications.
About Infineon Technologies AG
Infineon Technologies AG is a globally recognized leader in the semiconductor industry, particularly noted for its reliable and high-performance transistor technologies. In the realm of RF Small Signal Bipolar Transistors, Infineon consistently develops parts that meet diverse application needs ranging from automotive electronics to high-frequency telecommunication systems. The BFR93AE6327HTSA1 is just one example within a broader portfolio that exemplifies their commitment to quality and technological advancement. Infineon ensures that their transistors not only meet current market demands but also embrace future challenges with evolving technologies.
Where to Find BFR93AE6327HTSA1 by Infineon Technologies AG
To purchase the BFR93AE6327HTSA1, it’s recommended that customers use findchips.com. You can also explore alternate parts by searching within the RF Small Signal Bipolar Transistors category for similar components from Infineon or other manufacturers. Historically, this part has been supplied by distributors such as Win Source Electronics, EBV Elektronik, and Mouser Electronics. However, to ensure real-time availability and the best pricing, checking findchips.com is advisable.