QRE1113GR by onsemi

Overview of QRE1113GR by onsemi

The QRE1113GR is a reflective object sensor that combines an infrared emitter and a phototransistor detector in a single surface-mount device (SMD). Designed by onsemi, a leader in sensor technology, this component is optimized for detecting the presence of an object within a sensing distance of 5mm. The sensor’s output type is a phototransistor, which allows it to convert light intensity into a corresponding electrical output. This feature makes it suitable for a wide range of applications requiring precise object detection and distance measurement. Operating within a forward current (If) of 50mA and a collector emitter voltage (V(Br)Ceo) of 30V, the QRE1113GR is designed for low power consumption and high reliability in demanding environments.

Notable attributes of QRE1113GR include a maximum operating temperature of 85°C, a minimum of -40°C, and a quick response time of 20 µs. The sensor is also remarked for its ease of integration into systems due to its surface-mount design. Additionally, it is RoHS compliant, ensuring it meets global standards for environmental safety.

Industry Applications for QRE1113GR

The versatile nature of the QRE1113GR allows it to be a suitable component for various industry applications. Below are some potential use cases, although engineering and design teams should conduct thorough analysis and verification:

  • Industrial Automation: In assembly lines and machinery, the QRE1113GR could potentially serve as a precise object detection sensor, helping in the automation of manufacturing processes. For example, it might be used for detecting the presence or absence of parts in a production line, ensuring the correct assembly of products.
  • Robotics: Robots, especially those designed for sorting or logistics, could use the QRE1113GR for object sensing and distance measurement. This helps in pathfinding or in the accurate picking and placing of items.
  • Consumer Electronics: In devices requiring user interaction, such as gesture recognition or proximity sensing, the QRE1113GR can provide valuable input to the device’s control system.
  • Security Systems: The sensor might be incorporated into security devices, such as access control systems, where detecting the presence of an object or person is necessary for operation.

These applications leverage the QRE1113GR’s capacity for accurate sensing, low power consumption, and efficient response times, although specific implementations would require integration and testing within the target system.

About onsemi

onsemi is a renowned manufacturer in the field of semiconductors, particularly noted for its comprehensive range of sensors and transducers. Within the realm of Linear Position Sensors, onsemi offers a variety of components, including the QRE1113GR, that are designed to meet the diverse needs of modern industries. The company focuses on developing products that enhance energy efficiency, reduce global energy use, and offer lower costs of ownership. Their portfolio spans various types of sensors, including but not limited to, optical, temperature, position, and motion sensors, making onsemi a key player in enabling smarter, more connected solutions across a range of industries.

Where to Find QRE1113GR by onsemi

To purchase the QRE1113GR or to explore alternatives, one of the best resources available is findchips.com. Here, you can find real-time stock levels, pricing from multiple distributors, and detailed part information. For those interested in the broader category of Linear Position Sensors, this platform can also help identify alternate parts that might be offered by onsemi or other leading manufacturers.

In the past, the QRE1113GR has been available from various distributors including New Advantage Corporation, EBV Elektronik, Avnet Silica, Avnet Asia, Sensible Micro Corporation, Ameya Holding Limited, Quest Components, Bristol Electronics, Future Electronics, Mouser Electronics, Avnet Americas, DigiKey, and Newark. However, for the most current availability and pricing information, it is recommended that potential buyers refer directly to findchips.com.

Compare pricing for QRE1113GR and other Linear Position Sensors / Sensors/Transducers at findchips.com