MPXM2202AS by NXP Semiconductors

Overview of MPXM2202AS by NXP Semiconductors

The MPXM2202AS is an absolute, piezoresistive pressure sensor from NXP Semiconductors, featuring a sensitivity range from 0 to 200 kPa. This component is built for precision, offering a narrow error margin of 1% alongside an output voltage range of 0-40mV, ensuring accurate readings. The device operates between an ample temperature range of -40°C to 125°C, which supports versatility in challenging environments. Packaged in a rectangular surface mount style (MPAK-5), the MPXM2202AS facilitates integration into various schematic layouts. Its additional features include temperature compensation, which enhances the stability and reliability of the sensor in diverse operating conditions.

Characterized by a maximum supply voltage of 16V and minimum of 10V, this device requires a nominal current of only 6 mA. The sensor is RoHS compliant, guaranteeing adherence to environmental standards regarding hazardous substances. Its life cycle status is marked obsolete, so while it remains a viable option, alternative or next-generation solutions might also need to be considered.

Industry Applications for MPXM2202AS

The Pressure Sensors like MPXM2202AS find extensive utility across different sectors due to their precise measurement capabilities and robust performance in varied environmental conditions. Here are how industries could possibly benefit from integrating such sensors:

  • Environmental Monitoring: This sensor could potentially be utilized in weather stations for monitoring atmospheric pressure changes, aiding in climate study and weather forecasting models.
  • Industrial Automation: In automated systems that monitor and control industrial processes, the MPXM2202AS might be used to ensure optimal operations through continuous pressure measurement of gases and liquids.
  • Healthcare: Piezoresistive pressure sensors can be instrumental in medical devices that require precise control and monitoring of pressures, such as ventilators and blood pressure monitors.
  • Consumer Electronics: Employed in gadgets that adjust environmental settings based on atmospheric pressure, such as smart watches that include elevation tracking during hiking.

It’s important to note that these potential industry applications are only conceptual/illustrative and require thorough analysis and verification by engineering and design teams for compliance with industry standards and specific application requirements.

About NXP Semiconductors

NXP Semiconductors is recognized in the semiconductor industry primarily for its innovations and contributions to various high-tech sectors including automotive, industrial, and telecommunications. Within the realm of Sensors/Transducers, and specifically Pressure Sensors, NXP has developed a variety of parts, including the MPXM2202AS. The company focuses on devising robust, energy-efficient, and highly reliable products that cater to the growing demands of advanced electronic solutions. Their products typically integrate features that enhance usability, like temperature compensation and precise linearity, making them preferable choices in sectors where reliability and accuracy are paramount.

Where to Find MPXM2202AS by NXP Semiconductors

For current stock levels and pricing details of MPXM2202AS, I recommend checking on findchips.com. Additionally, by exploring the Pressure Sensors section, you can also discover alternate parts that might be offered by NXP Semiconductors or other manufacturers. Some of the distributers where this part has historically been available include Win Source Electronics, LCSC, Chip 1 Exchange, Rochester Electronics, Verical, Arrow Electronics, and Newark. Visit FindChips to get the most recent data relating to availability and competitive pricing.

Compare pricing for MPXM2202AS and other Pressure Sensors / Sensors/Transducers at findchips.com