Overview of DA16200MOD-AAC4WA32 by Renesas Electronics Corporation
The DA16200MOD-AAC4WA32 is an ultra-low power Wi-Fi module designed specifically for battery-powered IoT devices. This part, categorized under Other uPs/uCs/Peripheral ICs, operates on a 2.4GHz band and supports 1Mbps data rate. The module’s sensitivity is robust at -98.5 dBm, ensuring superior performance in environments with varying signal strength. Compliant with RoHS and having a peak reflow temperature of 260°C, this component adheres to current environmental and manufacturing standards.
Designed by Renesas Electronics, the DA16200MOD-AAC4WA32 is offered as part of a module package and is delivered in a 500-unit tape & reel format, indicative of its intended use in large-scale production environments. This component is in an active part life cycle stage, signifying ongoing manufacturer support and availability. As of the current writing, the factory lead time for this part is reported as 18 weeks.
Industry Applications for DA16200MOD-AAC4WA32
The DA16200MOD-AAC4WA32 finds its relevance across various industries due to its specialized characteristics for communication and power efficiency. These potential applications are broad but notably significant in particular sectors:
- Consumer Electronics: This module could potentially be integrated into smart home devices, such as wireless security cameras or thermostats, where efficient power use and reliable Wi-Fi connectivity are critical. The low-power consumption feature of the Wi-Fi module ensures longer battery life, which is paramount in these applications.
- Audio and Video Systems: The module might also be utilized in wireless audio devices, such as Bluetooth speakers or headphones. Consistent and robust Wi-Fi connectivity offered by the module supports a seamless streaming experience in audio and video systems.
- Entertainment and Gaming: In gaming devices where connectivity and extended battery life are necessary, this Wi-Fi module could considerably enhance user experience by facilitating consistent and uninterrupted gameplay, particularly in portable gaming consoles.
It is important to note that while these applications are conceptual, actual implementation should be validated by engineering and design teams to ensure compliance with industry standards and suitability for specific use cases.
About Renesas Electronics Corporation
Renesas Electronics Corporation is a key player in the field of Microcontrollers and Processors, with a particular strength in developing Other uPs/uCs/Peripheral ICs. Renesas is known for its innovative approach towards integrating complex system-on-chip designs that cater to a broad spectrum of industries. The DA16200MOD-AAC4WA32 is just one example of the company’s dedication to pushing the boundaries of what’s possible in the realms of connectivity and power efficiency. Their products typically integrate advanced technology which makes them favorable in high-demand applications throughout various tech sectors.
Where to Find DA16200MOD-AAC4WA32 by Renesas Electronics Corporation
To find the DA16200MOD-AAC4WA32 module, prospective buyers are encouraged to visit findchips.com. This site allows research on current stock levels and pricing across multiple distributors. Some previously known distributors of this part include Avnet Silica, Avnet Asia, Renesas Electronics America, Mouser Electronics, Avnet Americas, DigiKey, and Newark. Though this information is indicative of past availability, checking real-time data on findchips.com ensures up-to-date availability and pricing information. For alternatives to the DA16200MOD-AAC4WA32, the webpage for Other uPs/uCs/Peripheral ICs may also be consulted to discover similar parts by Renesas Electronics or other manufacturers.