Overview of PESD5V0S1BB,115 by Nexperia
The PESD5V0S1BB,115 is a bidirectional Electrostatic Discharge (ESD) protection diode designed for voltage suppression. It supports a maximum clamping voltage of 14V and operates at a nominal voltage of 5V. Housed in a SOD-523 package, it features 2 pins and boasts a power dissipation of 130W. This part is crafted from silicon, leveraging avalanche technology for robust voltage suppression, crucial for protecting sensitive electronic components from ESD damage.
Nexperia, the manufacturer, has ensured that this component complies with major industry standards such as IEC-60134 and IEC-61000-4-2, 4-5, indicating its suitability for stringent environments. This diode’s low capacitance feature makes it highly effective for protecting high-speed data lines against ESD without significantly impacting data integrity. Marketed primarily under the Transient Suppressors subcategory, the PESD5V0S1BB,115 shows compatibility with a wide range of applications owing to its versatile characteristics such as bidirectionality and 5V reverse voltage protection.
Industry Applications for PESD5V0S1BB,115
In today’s digitized world, components like PESD5V0S1BB,115 are potentially vital across various industries due to their protective characteristics. Below are selected industries where this diode might be particularly useful:
- Consumer Electronics: Devices such as smartphones, laptops, and other portable electronics might integrate these diodes to protect sensitive components from static electricity that can accumulate from regular human contact.
- Telecommunications: Equipment like routers, switches, and modems, which handle large volumes of data transfers and are sensitive to static charges, might benefit from the incorporation of such ESD protection diodes.
- Computing and Data Storage: High-performance servers which are vulnerable to numerous ESD events during their operational lifecycle might utilize these diodes to guard against these potentially damaging interactions.
- Healthcare: Medical devices and equipment that require rigorous protection against static discharges to ensure accurate functioning and reliability might also use similar diodes, although specific standards and certifications would be necessary for such applications.
Note: The potential applications of PESD5V0S1BB,115 outlined above are conceptual illustrations and should be carefully analyzed and verified by engineering and design teams to meet particular industry standards and specific requirements.
About Nexperia
Nexperia is a leader in the production of semiconductor components, specializing in areas like Diodes and specifically within the area of Transient Suppressors. The company produces components, such as the PESD5V0S1BB,115, that are known for their reliability and efficiency. Nexperia’s products are notable for their adherence to stringent industry standards such as IEC and RoHS, ensuring they meet global compliance requirements for safety and environmental impact. Through continuous innovation and focus on high-volume production of discrete and MOSFET components, Nexperia maintains its standing as a key supplier of industry-grade electronic components. The company’s expertise in specific areas such as ESD protection diodes helps clients across multiple sectors safeguard the operational stability and longevity of high-tech electronic systems.
Where to Find PESD5V0S1BB,115 by Nexperia
To procure the PESD5V0S1BB,115 diode, it is advisable to conduct thorough research regarding availabilities and pricing through a reputed distributor aggregator like findchips.com. Interested buyers can also explore other Transient Suppressors, which might be available from Nexperia or other manufacturers. In the past, this part has been stocked by distributors including New Advantage Corporation, EBV Elektronik, DigiKey, and Mouser Electronics, among others. However, for the latest availability and most competitive pricing, checking the current listings on findchips.com is recommended.