188744-1 by TE Connectivity

Overview of 188744-1 by TE Connectivity

The 188744-1 is a crimp receptacle contact designed for discrete wire applications. This specific part is manufactured by TE Connectivity and features female contact gender, making it suitable for various connector configurations. The part is typically used with wire gauges ranging from 28 to 24 AWG, providing flexibility in different wiring situations. The contact is made from phosphor bronze and has a tin-plated finish, which helps enhance its conductivity and resistance to corrosion.

This contact component is part of the Assembly Items subcategory within the broader category of Connector Support. The component is designed for signal applications and has a rated current of 3 A, which allows for its use in moderate power applications. It can operate within a temperature range of -40 °C to 100 °C, making it suitable for various environmental conditions. The cable entry requirements range from 0.032 inch to 0.059 inch, adding further versatility in installation.

As of the current writing, the factory lead time for the 188744-1 is approximately 16 weeks and 4 days. The part is compliant with REACH regulations and is also RoHS compliant, ensuring it meets certain environmental standards.

Industry Applications for 188744-1

The 188744-1 could potentially be utilized across various industries due to its design and properties. Below are some example applications where this part might be considered:

  • Internet of Things (IoT): In IoT devices, the ability to manage signal connection through discrete wiring is crucial. The 188744-1 might be used in sensor modules or other signal processing units, where a reliable electrical connection is required.
  • Industrial Automation: This contact may also find applications in industrial automation systems, such as those used in manufacturing equipment or automated assembly lines. Its rated current allows for the support of control signals and communication between devices.
  • Transportation and Logistics: In the transportation sector, the 188744-1 could be utilized in vehicle communication systems where durable and reliable connectors are necessary for transmitting signals, especially in harsh environments.
  • Consumer Electronics: The contact might be used in consumer electronic devices where discreet connections are essential, such as in portable electronic devices. This could include audio equipment and wearable technology.
  • Robotics and Drones: In robotics, the 188744-1 could potentially be employed within control circuits in robotic arms or drones, where lightweight and compact wiring solutions are required.

It should be noted that these potential industry applications are only conceptual and illustrative. Engineering and design teams must analyze and verify adherence to industry standards and specific application requirements before employing the 188744-1 in any particular use case.

About TE Connectivity

TE Connectivity is a global leader in connectivity and sensor solutions, providing products that support a range of industries. Within the specific area of Assembly Items, TE Connectivity offers various connector support components, including the 188744-1. The company focuses on quality and reliability in their designs, with similar products that ensure robust connections for diverse applications.

TE Connectivity’s portfolio includes various types of connectors and accessories that might also be suitable for applications in conjunction with the 188744-1, ensuring design flexibility and performance in demanding environments. The commitment to innovation ensures that they stay at the forefront of connector technology.

Where to Find 188744-1 by TE Connectivity

To purchase the 188744-1, you can research various distributors listed on findchips.com. Some distributors that have historically carried this part include:

  • NTEMALL
  • Master Electronics
  • DigiKey
  • Avnet Americas

Be advised that stock availability may vary, and it is recommended to check findchips.com for the most current stock levels and pricing. Additionally, you can also explore the Assembly Items category to find alternate parts that might be offered by TE Connectivity or other manufacturers.

Compare pricing for 188744-1 and other Assembly Items / Connector Support at findchips.com