Overview of 2907665 by Phoenix Contact
The 2907665 is a thermal magnetic circuit breaker designed for electrical circuit protection. It has a current rating of 20A and operates at voltage levels up to 480VAC and 125VDC, making it suitable for various applications requiring reliable circuit interruption. This component belongs to the circuit breaker subcategory within the larger category of circuit protection, which plays a crucial role in safeguarding electrical systems from overcurrent conditions.
Manufactured by Phoenix Contact, a company known for its innovative electronic components, the 2907665 is part of the TMC 82D series of circuit breakers. This series features thermal magnetic technology, combining both thermal and magnetic protection mechanisms, which collectively provide effective circuit interruption in various fault conditions. The thermal mechanism is primarily responsible for protecting against overcurrent situations, while the magnetic mechanism responds swiftly to short circuit occurrences.
As of this writing, the 2907665 is active in the market and demonstrates compliance with industry standards, including ROHS and REACH regulations, ensuring that it meets environmental and safety guidelines. The part’s lifecycle status indicates that it is not obsolete and is supported by the manufacturer, thus making it a viable option for sourcing in ongoing projects.
Industry Applications for 2907665
The 2907665 circuit breaker may potentially find applications across various industries. Below are some examples of where this part might be utilized:
- Industrial Automation: This part could be used in automated systems, such as conveyor systems or robotics, where reliable circuit protection is necessary to prevent equipment damage during electrical faults.
- Telecommunications: The 2907665 might be suitable for telecommunications infrastructure, protecting sensitive communication equipment from voltage surges and current overloads.
- Aerospace and Defense: Although specific military standards were not provided, thermal magnetic circuit breakers like this one could support satellite and aerospace applications where power distribution and fault protection are critical. Note that such use cases would require adherence to relevant military or aerospace standards.
- Consumer Electronics: The component might potentially be integrated into consumer electronic products that operate at the specified voltage and current ratings, providing protection against overcurrents that could damage sensitive electronic components.
- Transportation and Logistics: It may also be applicable in transportation systems, like electric vehicle charging stations, where protection against electrical overload is vital for safety and reliability.
It is important to note that these potential industry applications are only conceptual and illustrative. Engineering and design teams should conduct thorough analyses and verifications to ensure adherence to industry standards and specific application requirements before deciding on the implementation of the 2907665.
About Phoenix Contact
Phoenix Contact is a leading manufacturer in the field of electrical engineering, particularly known for its innovative products in circuit protection, including thermal magnetic circuit breakers. The company emphasizes quality and reliability in its components. Within the realm of circuit breakers, the 2907665 exemplifies their commitment to providing robust solutions for a plethora of industries. Phoenix Contact also manufactures similar parts that cater to various specific circuit protection needs, ensuring different applications can leverage their expertise in circuit design and protection technology.
Where to Find 2907665 by Phoenix Contact
If you are interested in purchasing the 2907665, it is advisable to research current stock levels and pricing options from various suppliers. You can visit findchips.com for detailed information about availability. Historically, the part has been available at distributors such as:
- Neutron USA
- Master Electronics
- Sager
- TTI
- Onlinecomponents.com
- Mouser Electronics
- DigiKey
However, keep in mind that stock availability may fluctuate, so checking findchips.com is essential for the most accurate and up-to-date information.