Overview of FKN50SJR-52-10R by YAGEO Corporation
The FKN50SJR-52-10R is a 10-ohm wire wound resistor designed for axial lead applications. It features a resistance tolerance of ±5% and a power rating of 500 mW, making it suitable for various electronic applications where precision is needed. The resistor has a rated working voltage of 200V, which provides a robust option for circuits that require voltage stability. This part is constructed in a tubular shape, enhancing its heat dissipation capabilities, and is designed for through-hole mounting.
Notably, the FKN50SJR-52-10R is a fusible flame-proof resistor, which is important for applications where safety is a major concern. It is rated to withstand temperatures from -40 °C to a maximum of 275 °C, and its construction adheres to safety standards set by UL (Underwriters Laboratories). This means that in the event of an overload, the resistor is designed to fail safely, thereby protecting other components in the circuit. The part also meets RoHS and REACH compliance, indicating that it is free from hazardous substances and complies with environmental regulations.
As of the current writing, the factory lead time for this part is approximately 24 weeks, which is essential to consider for procurement and planning purposes.
Industry Applications for FKN50SJR-52-10R
The FKN50SJR-52-10R could potentially be applicable across various industries where precise resistance and reliability are crucial. Here are some example industries where this component might be utilized:
- Consumer Electronics: In consumer electronics, the FKN50SJR-52-10R might be used in power supply circuits or as a current-limiting resistor. The resistor’s flame-proof feature could provide extra security in devices that draw significant current.
- Telecommunications: In telecommunications equipment, this resistor could serve as part of signal conditioning circuits. Its tight tolerance and stability across a wide temperature range might assist in maintaining the integrity of signals.
- Environmental Monitoring: This resistor might find its application in devices employed for environmental monitoring, possibly as part of sensing circuits that require accurate readings under varying conditions.
- Healthcare: In medical devices, the fusing characteristic of the FKN50SJR-52-10R could play a vital role in protecting sensitive components from unexpected power surges.
- Smart Cities: For smart city applications, this resistor could be used in IoT devices where reliability and safety are paramount given their connection to critical infrastructure.
It is important to note that these potential industry applications are only conceptual and require analysis and verification by engineering and design teams for adherence to industry standards and specific application requirements.
About YAGEO Corporation
YAGEO Corporation is a leading manufacturer of resistors, capacitors, and inductors, with a significant focus on innovative electronic components. The company has a diverse portfolio, including the FKN50SJR-52-10R wire wound resistor and similar products aimed at various industries. Their commitment to quality, as demonstrated by compliance with safety standards such as UL, enhances their credibility in the marketplace.
YAGEO’s wire wound resistors are characterized by their stability and high precision, making them suitable for applications where reliability plays a crucial role. The FKN50SJR-52-10R aligns with the company’s focus on producing durable components that comply with global environmental norms. Similar parts in their catalogue may include various ohmic values and power ratings designed to meet diverse needs in electronic assemblies.
Where to Find FKN50SJR-52-10R by YAGEO Corporation
For procurement, it is advisable to research where to purchase the FKN50SJR-52-10R. Check the listings on our site findchips.com, which may provide useful information about current stock levels and pricing. This part has historically been available at several distributors, including:
- Ozdisan Elektronik
- Avnet Abacus
- TTI
- Future Electronics
- Mouser Electronics
- Avnet Americas
- DigiKey
While these distributors have previously stocked the FKN50SJR-52-10R, it is important to confirm current availability on findchips.com, as stock levels may vary.