413985-3 by TE Connectivity

Overview of 413985-3 by TE Connectivity

The part 413985-3 is a straight plug connector designed for RF (radio frequency) applications, specifically categorized as an RF SMB Connector. This component features a characteristic impedance of 50 ohms, which is essential for maintaining signal integrity in RF applications. The plug assembly is constructed using materials such as brass for the shell, which is nickel-plated for corrosion resistance, and polytetrafluoroethylene (PTFE) for the insulator. This ensures durability and reliable performance across various applications.

As a crimp termination type, the 413985-3 is designed to connect various cable types including RG 174, RG 316, RG 188, and RG 188A, which are commonly used in RF and communication systems. The insertion loss at 3 GHz is a maximum of 0.3 dB, which signifies minimal signal degradation when passing through the connector. This part is RoHS compliant, indicating that it meets environmental standards regarding hazardous substances.

Additional attributes include a wide operating temperature range from -65 °C to 165 °C and an operating frequency maximum of 4 GHz. This allows the 413985-3 to function effectively in diverse environments and applications. The connector’s life cycle status is active, and the factory lead time is currently noted at five days. Engineers and procurement professionals can consider these factors when assessing the suitability of this component for their specific applications.

Industry Applications for 413985-3

The RF SMB connector, such as the 413985-3, has applicability in various industries. Below are some potential use cases where this connector might be utilized:

  • Telecommunications: The part could be integrated into communication devices and infrastructure that require reliable signal transmission. For example, this connector might be used in base stations, antennas, or RF transceivers, which demand low insertion loss and robust performance.
  • Consumer Electronics: This connector might also find its way into consumer products that rely on RF signals, such as televisions or wireless audio systems. The ability to maintain performance at an operating frequency of up to 4 GHz could support streaming services and other high-frequency uses.
  • Industrial Automation: The 413985-3 could potentially be used in automation equipment that communicates wirelessly or collects data via sensors. The connector’s durability and wide temperature range may suit applications in demanding environments, possibly enhancing system reliability.
  • Healthcare Technology: In medical imaging or diagnostic equipment, this connector could be used due to its low insertion loss and compliance with certain industry standards. While not explicitly listed, the attributes may allow for its use in devices that transmit RF signals for monitoring and imaging purposes.
  • Aerospace and Defense: Although specific MIL standards were mentioned, the robust nature of the connector might support use in aviation communication systems. Its ability to operate in extreme temperatures could make it suitable for applications within aircraft and satellites.

These potential industry applications are only conceptual/illustrative and require analysis and verification by engineering and design teams for adherence to industry standards and specific application requirements. Similar connectors in the RF SMB category might also serve these applications and could provide alternative solutions.

About TE Connectivity

TE Connectivity is a significant player in the connector manufacturing industry, specializing in various types of connectors, including RF connectors like the 413985-3. With a focus on quality and performance, TE Connectivity’s RF SMB/SSMB connectors are designed to meet the rigorous demands of modern electronic systems. The company offers a range of similar parts that cater to different applications, ensuring that engineers have access to reliable components for their projects. TE Connectivity’s commitment to innovation and quality positions them as a trusted manufacturer in the electronics market, particularly in the domain of RF connectors.

Where to Find 413985-3 by TE Connectivity

findchips.com as a resource for current stock levels and pricing. The site can also direct you to alternative RF SMB/SSMB connectors, which can be found by exploring the RF SMB/SSMB Connectors category. Historically, distributors like Master Electronics, DigiKey, Mouser Electronics, and Avnet have had availability of this connector. However, users should verify the current stock and pricing directly on findchips.com to ensure the best buying decisions.

Compare pricing for 413985-3 and other RF SMB/SSMB Connectors / Connectors at findchips.com