FSA2567MPX by onsemi

Overview of FSA2567MPX by onsemi

The FSA2567MPX is an innovative component developed by onsemi, catering to a relatively specific niche within the realm of electronic parts. It is a Low Power, Dual SIM Card Analog Switch, showcased in a 3000-reel package for efficient distribution and assembly. Manufactured in a MLP-16 (Micro Leadframe Package – 16 leads) package, this part promises a compact footprint alongside robust operation characteristics. The device is specifically designed to facilitate the switching between dual SIM (Subscriber Identity Module) card operations, making it a vital component in devices requiring multi-SIM functionalities.

With a focus on preserving energy, the FSA2567MPX operates under a minimal power requirement regime, supporting a broad range of supply voltages from 1.65 V to a maximum of 4.3 V. This flexibility enables the switch to easily integrate into various circuit designs without necessitating major power supply adjustments. Additionally, the package boasts a moisture sensitivity level of 1, providing an indicator of its resilience and durability in varied environmental conditions.

Technical parameters of note include an on-state resistance (Ron) maximum of 12 Ω, off-state isolation nominal of 60 dB, and a break-before-make switching mechanism, ensuring reliable disconnection and connection between circuits. The part also demonstrates quick switching times, with a switch-off time maximum of 50 ns and a switch-on time maximum of 95 ns, contributing to efficient operation in use cases demanding rapid switching between SIM cards.

Industry Applications for FSA2567MPX

The dual SIM card feature enabled by FSA2567MPX positions this component as a valuable asset across multiple industries. While consumer electronics stand at the forefront of applications, the versatility provided by this switch opens the door to a broader range of use cases. Following are some potential application scenarios, bearing in mind the need for design and engineering validations:

  • Mobile Devices: Smartphones and tablets with dual SIM functionalities might employ FSA2567MPX to manage active connections with more than one network provider simultaneously, enhancing user flexibility and network coverage.
  • Wearable Technology: Wearable devices such as smartwatches equipped with cellular capabilities could utilize FSA2567MPX to switch between different network providers or manage different profiles, depending on the usage or geographic scenario.
  • Automotive Communications: Vehicles with integrated eSIM technology for global connectivity solutions might integrate the FSA2567MPX for managing connections between different network operators, particularly in international models that require connectivity across borders.
  • Internet of Things (IoT) Devices: IoT devices requiring uninterrupted connectivity could benefit from the dual SIM management capabilities of FSA2567MPX, ensuring persistent data exchange even if one network becomes unavailable.

It is important to note that these applications are speculative and should be subjected to thorough analysis by engineers and designers to ensure compatibility and performance within specific use cases.

About onsemi

onsemi stands as a key player in the domain of semiconductor solutions, with a keen focus on improving energy efficiency across a myriad of electronic applications. Within the Multiplexers or Switches category, onsemi’s portfolio includes innovative components like the FSA2567MPX, among others, tailored for precise and efficient signal routing. The manufacturer distinguishes itself through continuous innovation and dedication to quality, developing parts that address the critical needs of the industry’s evolving demands. Their offerings span across various functionalities within Signal Circuits, contributing to onsemi’s reputation as a provider of comprehensive semiconductor solutions.

Where to Find FSA2567MPX by onsemi

For those interested in procuring the FSA2567MPX, findchips.com serves as a reliable tool for identifying current stock levels, pricing, and available distributors. Recognizing that electronic component needs can be both immediate and specific, findchips.com consolidates distributor information into a single platform, simplifying the procurement process. As of historical data, distributors such as New Advantage Corporation, LCSC, EBV Elektronik, and CHIPMALL.COM LIMITED have been known to stock the FSA2567MPX. However, the availability can fluctuate, and for this reason, potential purchasers are encouraged to visit findchips.com to access up-to-date information.

Additionally, for those exploring alternatives within the realm of Multiplexers or Switches or seeking parts with similar functionalities offered by onsemi or other manufacturers, findchips.com offers a comprehensive searchable database. This tool aids in comparing multiple options, ensuring that procurement decisions are both informed and strategic.

Compare pricing for FSA2567MPX and other Multiplexers or Switches / Signal Circuits at findchips.com