12191818 by Aptiv PLC

Overview of 12191818 by Aptiv PLC

The part 12191818 is a push-on terminal designed for automotive applications, particularly within the Aptiv GT 150 Series. This terminal features a socket contact and utilizes a crimp termination type, accommodating wire sizes of 0.5 mm². It is specifically engineered for integration with the Aptiv GT 150 Series automotive housing connectors. One important aspect of this component is its compliance with RoHS standards, which indicates that it adheres to regulations regarding hazardous substances in electrical and electronic equipment.

In terms of its physical attributes, this terminal is categorized under the electronic parts subcategory of Terminals and Terminal Blocks. Additionally, the part has a life cycle code indicating it remains active within the manufacturer’s portfolio. While details regarding reach compliance are not extensively documented, it is essential to verify such attributes during the procurement process.

Industry Applications for 12191818

The 12191818 terminal could find potential applications across various industries due to its specifications and compatibility with automotive housing connectors. Below are some possible use cases that illustrate the versatility of this component:

  • Automotive: Given its design for the GT 150 Series, this terminal might be utilized in vehicle wiring harnesses for connecting electrical systems. It may support functions such as power distribution, sensor integration, and control unit connectivity.
  • Industrial Automation: The robust nature of the 12191818 terminal could potentially serve in industrial automation systems. For example, it might be part of a connection interface for programmable logic controllers (PLCs) or sensors in automated machinery.
  • Consumer Electronics: The terminal could possibly be used in the assembly of consumer electronic devices requiring reliable electrical connections, such as laptops or gaming consoles, particularly if these devices have automotive-like functionality.
  • Telecommunications: In telecommunications equipment, the 12191818 terminal might support low-voltage connections, enabling communication devices to maintain operational integrity in rugged environments.
  • Robotics and Drones: The compact format and crimp termination of this terminal could make it suitable for connecting components within drones or robotic systems, where space and weight considerations are critical.

These potential industry applications are only conceptual and illustrative. Careful analysis and verification by engineering and design teams are necessary to ensure adherence to specific industry standards and application requirements. It may be prudent to consider the entire context in which the 12191818 terminal will function.

About Aptiv PLC

Aptiv PLC is a global technology company focused on developing safer, greener, and more connected solutions for a variety of automotive applications. As a prominent manufacturer in the field of connectors, Aptiv specializes in high-performance solutions that facilitate robust and reliable electrical connections. The company’s offerings include a wide range of terminals and terminal blocks, particularly under the GT series, which emphasizes clean, secure, and easily deployable connections.

The 12191818 terminal is part of this GT 150 Series, and Aptiv manufactures other similar parts aimed at meeting the diverse needs of automotive and industrial markets. By leveraging advanced materials and manufacturing processes, Aptiv aims to enhance the scalability and reliability of their connector solutions, thereby supporting innovation within automotive design and manufacturing.

Research Price and Stock for 12191818 by Aptiv PLC on Findchips.com

For readers interested in purchasing the 12191818 terminal, it is recommended to conduct a thorough search for stock and pricing on Findchips. This platform can provide insights into current stock levels and market pricing for the part, which can fluctuate based on distributor availability and demand.

Historical availability of the 12191818 terminal has been noted at various distributors, including:

  • Master Electronics
  • Avnet Abacus
  • TME
  • TTI
  • Onlinecomponents.com
  • Mouser Electronics
  • Newark

However, it is essential to check Findchips for the latest availability and pricing updates, as stock can change frequently based on market conditions.

Compare pricing for 12191818 and other Terminals and Terminal Blocks at findchips.com