KW-5R5C105-R by Eaton Corporation

Overview of KW-5R5C105-R by Eaton Corporation

The KW-5R5C105-R is an Electric Double Layer Capacitor (EDLC), commonly referred to as a supercapacitor or ultracapacitor, with a substantial capacity of 1.0 farad and a rated voltage of 5.5 volts. This component is characterized by its wide operating temperature range from -40°C to 85°C, making it suitable for various challenging environments. Manufactured by Eaton Corporation, the capacitor is housed in a radial leaded, cylindrical package that measures 21.5mm in diameter and 8.85mm in length. It is designed for through-hole mounting, features terminals with a pitch of 5mm, and is halogen-free and RoHS compliant. The capacitance tolerance is notably broad, with a positive tolerance of +80% and a negative tolerance of -20%, emphasizing its ability to maintain performance under varying conditions. Additionally, its durability is underscored by its operational lifespan of 2000 hours at 85°C.

Eaton Corporation’s KW-5R5C105-R falls within the Special Capacitors subcategory, distinguishing itself with its substantial energy storage capacity and robust design. These features make it an integral component in applications requiring rapid charge and discharge cycles over short periods, energy backup, and power smoothing functionalities.

Industry Applications for KW-5R5C105-R

The KW-5R5C105-R’s unique characteristics such as high capacity and durability, align it with a multitude of potential industry applications. While its specific utility needs to be meticulously analyzed and verified by engineering and design teams, the following are illustrative applications within several industries:

  • Consumer Electronics: The KW-5R5C105-R could potentially be used in portable consumer electronics devices for power backup or quick charge situations. Devices such as digital cameras, smartphones, and portable power banks might benefit from the quick energy release and charging capabilities of this supercapacitor.
  • Energy and Power Systems: In the energy sector, supercapacitors like the KW-5R5C105-R can provide critical benefits in terms of power quality, energy efficiency, and reliability. For example, they might be utilized in uninterruptible power supply (UPS) systems to provide short-term backup power or to help stabilize voltage and smooth out interruptions in grid operations.
  • Renewable Energy Systems: Supercapacitors are increasingly relevant in renewable energy applications, including solar power and wind energy systems, where they can store excess energy and release it when generation is low. The KW-5R5C105-R could serve as a buffer to manage energy flow, enhance efficiency, and contribute to the stability of renewable energy installations.

These potential applications illustrate the versatility and relevance of the KW-5R5C105-R across various sectors. However, it’s crucial for teams to conduct thorough feasibility studies and engineering evaluations to ensure its compatibility and optimal performance within specific applications.

About Eaton Corporation

Eaton Corporation is a globally recognized leader in the development and manufacturing of electronic components, specializing in a wide range of capacitors, including Special Capacitors. Within this domain, the Eaton Corporation designs and produces components that find essential use across diverse industrial, commercial, and consumer applications. The KW-5R5C105-R is a testament to Eaton’s commitment to delivering innovative, reliable, and effective energy storage solutions. Eaton’s portfolio includes a variety of capacitors tailored to specific needs, ranging from general-purpose applications to specialized sectors where performance under extreme conditions is critical. This breadth of offerings underscores Eaton’s expertise and leadership in the capacitor market, making their components highly sought after for their quality, durability, and technological advancement.

Where to Find KW-5R5C105-R by Eaton Corporation

To locate the KW-5R5C105-R for purchase, findchips.com offers an extensive database that includes current stock levels, pricing, and availability from a plethora of distributors. Historically, this component has been available through distributors such as Avnet Asia, Avnet Abacus, TTI, Onlinecomponents.com, Future Electronics, and Mouser Electronics. However, stock availability can fluctuate. Hence, prospective buyers are encouraged to use Findchips to access the most recent data. Additionally, for those seeking alternate parts or components offered by Eaton Corporation and other manufacturers within the domain of Special Capacitors

, Findchips serves as an invaluable resource for comparison shopping, ensuring that procurement professionals and engineers can make informed decisions based on the latest information.

Compare pricing for KW-5R5C105-R and other Special Capacitors / Capacitors at findchips.com