CC0603JRNPO9BN470 by YAGEO Corporation

Overview of CC0603JRNPO9BN470 by YAGEO Corporation

The CC0603JRNPO9BN470 by YAGEO Corporation is a multilayer ceramic capacitor (MLCC) in the 0603 package size, which corresponds to 1.6mm x 0.8mm (length x width) with a thickness of 0.034 inches (approximately 0.86mm). This capacitor offers a capacitance of 47 pF with a capacitance tolerance of ±5%, operating within the C0G (NP0) dielectric characteristic. It is designed for a rated DC voltage of 50V and capable of functioning over a wide temperature range from -55ºC to +125ºC. The capacitor is ROHS compliant, ensuring its suitability for applications demanding environmentally safe components.

The C0G (NP0) temperature characteristic of this capacitor denotes a very stable capacitance value across its entire operating temperature range, with a temperature coefficient of 30 ppm/°C, making it an excellent choice for precision applications where temperature stability is critical. The MLCC is packaged on a 7″ reel using paper tape, which aids in automated assembly processes, and it is designed for surface-mount technology (SMT) with a rectangular shape and wraparound terminal shape. Being rated as active in its part life cycle and having a lead time of 21 weeks as of the current writing, the CC0603JRNPO9BN470 remains a viable choice for new designs and production needs.

Industry Applications for CC0603JRNPO9BN470

Given its electrical characteristics and package size, the CC0603JRNPO9BN470 capacitor might potentially be used across various industry sectors. Below are some key industry applications where this component could find utility. It’s important to note that the specifics of use within these domains would require careful consideration by engineering and design teams to ensure compliance with industry standards and specific application requirements.

  • Consumer Electronics: This ceramic capacitor could potentially be used in devices such as smartphones, tablets, and wearables, where stability across a wide temperature range might be crucial for the device’s functionality and battery life.
  • Industrial Control: In industrial settings, the CC0603JRNPO9BN470 could be beneficial for control circuitry in machinery and equipment that operate in environments with varying temperatures, where precision and stability are required for effective operation.
  • Telecommunications: This capacitor might find applications in the telecommunications sector, possibly within RF circuitry, where its stable performance across temperature variations and tight capacitance tolerance are valuable for signal integrity.
  • Education and Research: Within academic and research laboratories, the CC0603JRNPO9BN470 might be utilized in experimental setups and projects that involve detailed electronic component studies, given its precise capacitance and stability characteristics.

These potential industry applications are illustrative and require thorough analysis and verification by relevant professionals to ensure suitability based on technical specifications and regulatory compliance.

About YAGEO Corporation

YAGEO Corporation is a global leader in the manufacture of a wide range of electronic components, with a significant focus on passive components such as resistors, capacitors, and wireless components. Within the realm of Ceramic Capacitors, YAGEO offers an extensive product line that caters to various industries and applications. The CC0603JRNPO9BN470 is just one example of YAGEO’s commitment to quality and innovation in ceramic capacitor technology. YAGEO’s products are known for their reliability, precision, and performance, serving as foundational elements in a wide array of electronic devices and systems across the globe.

Where to Find CC0603JRNPO9BN470 by YAGEO Corporation

To purchase the CC0603JRNPO9BN470 ceramic capacitor or to find similar parts, findchips.com is an invaluable resource. By using the Ceramic Capacitors link, one can also explore alternate parts offered by YAGEO Corporation or other manufacturers, which might be more suitable for specific applications. Historically, distributors such as DigiKey, Mouser Electronics, Newark, and Future Electronics have stocked this component. However, for current stock levels, pricing, and possible alternative sources, checking real-time data on findchips.com is highly recommended.

Compare pricing for CC0603JRNPO9BN470 and other Ceramic Capacitors / Capacitors at findchips.com