AD688ARWZ by Analog Devices Inc

Overview of AD688ARWZ by Analog Devices Inc.

The AD688ARWZ is a high precision ±10 V reference voltage source, designed and manufactured by Analog Devices Inc. This component belongs to the Voltage References subcategory within the Power Circuits category, designed for applications that demand high accuracy and stability. The AD688ARWZ operates within a temperature range of -40°C to +85°C, making it suitable for a wide range of industrial applications.

Key features of the AD688ARWZ include an initial accuracy of 4mV and a temperature coefficient of 8ppm/°C. This device is housed in a WSOIC-16 package with a total of 16 pins for connection. The output voltage ranges nominally around 10 V, with a minimal deviation verifying its precision. It is designed for a supply voltage between 13.5 V to 18 V. The specification for moisture sensitivity level 1 indicates its robustness for various environmental conditions. Additionally, the AD688ARWZ is RoHS compliant, ensuring it meets current environmental standards regarding the restriction of hazardous substances.

Industry Applications for AD688ARWZ

The AD688ARWZ by Analog Devices Inc. can potentially be integrated into various industry applications, owing to its high precision and stability in voltage reference. These applications span across several fields, reflecting the versatility of this component. Note that the following potential industry applications are purely conceptual/illustrative and require thorough analysis and verification by engineering and design teams to ensure compatibility with specific requirements and adherence to industry standards.

  • Education and Research: In laboratory settings, the AD688ARWZ might serve as a stable voltage source for precision measurement equipment, facilitating experiments and studies that require accurate voltage references.
  • Internet of Things (IoT): For IoT devices that monitor environmental conditions or perform critical data acquisitions, the precise voltage reference provided by the AD688ARWZ could ensure accurate sensor readings and reliable operation.
  • Computing and Data Storage: In systems where data integrity and accuracy are crucial, such as in data centers, the AD688ARWZ could potentially be used to enhance the reliability of power supplies and signal conversion processes.
  • Aerospace and Defense: Given the extreme conditions and the need for uncompromising accuracy in aerospace and defense applications, the AD688ARWZ might be used in navigation systems, monitoring equipment, and other critical electronic components.

Note these potential applications are provided for conceptual understanding and must be validated for technical and compliance aspects by the relevant professionals before implementation.

About Analog Devices Inc.

Analog Devices Inc. is a leader in the design and manufacturing of analog, mixed-signal, and DSP integrated circuits that address a wide range of applications from analog and digital signal processing to power management and Internet of Things (IoT). Within the realm of Voltage References and Power Circuits, Analog Devices Inc. showcases its expertise through products like the AD688ARWZ and similar parts, which are celebrated for their precision, reliability, and efficiency. Analog Devices Inc. excels in creating components that are critical to innovation in digital healthcare, automotive technology, digital communication and connectivity, and much more, consistently pushing the boundaries of technology to solve complex challenges and empower intelligent systems worldwide.

Where to Find AD688ARWZ by Analog Devices Inc

To procure the AD688ARWZ by Analog Devices Inc., potential buyers are encouraged to explore our site findchips.com. We provide access to current stock levels and pricing from various distributors, ensuring that you can find the most up-to-date and competitive offerings. Historically, the AD688ARWZ has been available through distributors such as Chip1Stop, Richardson RFPD, Quest Components, Analog Devices Inc., Mouser Electronics, DigiKey, and Newark. However, to ensure availability and current pricing, users should consult findchips.com.

For those seeking alternatives or variations of the AD688ARWZ that might be offered by Analog Devices Inc. or other manufacturers, the Voltage References section on findchips.com is an excellent resource for exploring a wide range of similar parts. This feature aids in comparative analysis, ensuring that you select the best component for your specific application needs.

Compare pricing for AD688ARWZ and other Voltage References / Power Circuits at findchips.com