Overview of LSM6DSVTR by STMicroelectronics
The LSM6DSVTR from STMicroelectronics is an analog circuit Inemo inertial module, designed to be implemented into a wide variety of applications requiring accurate detection of motion, acceleration, and angular rate. This component integrates both a tri-axis gyroscope and a tri-axis accelerometer on the same chip, providing a comprehensive solution for motion sensing needs. Its ability to operate across a supply voltage range from 1.71V to 3.6V makes it versatile for many electronic designs. Encased in an LGA-14 package, this MEMS (Micro-Electro-Mechanical Systems) module ensures a compact footprint while offering high functionality and reliability for various applications.
Its product range is expansive with a sensor case styled in LGA (Land Grid Array), featuring 14 pins for connectivity. Being RoHS compliant, the LSM6DSVTR adheres to strict environmental standards, minimizing the use of hazardous substances in electronic components. As part of the Other Signal Circuits subcategory, this part signifies an adherence to quality and regulatory compliance, poised for integration in globally marketed devices. As of the current writing, the part is in an active lifecycle phase with a factory lead time of 16 weeks, indicating continuous production and availability but necessitating planning for supply chain management.
Industry Applications for LSM6DSVTR
The LSM6DSVTR module’s integration of both tri-axis gyroscope and tri-axis accelerometer capabilities allows for its application across a broad spectrum of industries. This versatility is underpinned by its robust feature set, which includes low power consumption, high precision, and a compact form factor. Though the possibilities are vast, below are some key industries and potential use cases for this part:
- Consumer Electronics: Possessing the capabilities for enhancing user interfaces through motion detection and gesture recognition, the LSM6DSVTR could potentially be incorporated into smart devices like wearables, smartphones, and game controllers to provide improved interaction experiences.
- Internet of Things (IoT): In IoT devices, accurate motion sensing is crucial for applications such as indoor positioning, security systems, and activity tracking. The LSM6DSVTR might offer the precision and low power operation needed for these battery-powered devices.
- Audio and Video Systems: Stabilization and orientation features are critical in cameras and drones. The LSM6DSVTR could provide these functionalities, significantly enhancing the quality of video recordings by stabilizing footage and orientating the device.
- Agriculture Technology: For precision farming equipment that requires orientation and motion detection to navigate and perform tasks, the LSM6DSVTR’s accelerometer and gyroscope functionalities could offer valuable data inputs for automation and efficiency.
Note that these potential industry applications are only conceptual/illustrative and require rigorous analysis and verification by engineering and design teams to ensure adherence to industry standards and specific application requirements.
About STMicroelectronics
STMicroelectronics is a global semiconductor leader delivering intelligent and energy-efficient products and solutions that power the electronics at the heart of everyday life. Within the realm of Other Signal Circuits, STMicroelectronics has established a name for itself by developing and distributing a vast array of components, including various MEMS modules like the LSM6DSVTR. Their commitment to innovation is seen in the continuous improvement of their product offerings, incorporating advanced features and capabilities to meet the demanding requirements of the electronics industry.
The company’s prowess in designing signal circuits and other semiconductor products stems from its extensive research and development efforts. By focusing on the future of electronics, STMicroelectronics ensures its products, such as the LSM6DSVTR, are equipped with the latest technologies that provide reliability, performance, and value to its customers globally. Their comprehensive portfolio encompasses a wide range of products catering to diverse applications, from automotive and industrial to consumer electronics and emerging IoT devices.
Where to Find LSM6DSVTR by STMicroelectronics
For engineering or procurement professionals looking to source the LSM6DSVTR by STMicroelectronics, the best resource available is findchips.com. This platform provides up-to-date information on availability, pricing, and sourcing options from various distributors. Historically, the LSM6DSVTR has been available at distributors such as Future Electronics, STMicroelectronics, Mouser Electronics, Avnet Americas, DigiKey, and Newark, among others. However, potential buyers should visit findchips.com to get the current stock levels and pricing from these and other distributors.
Additionally, for those seeking alternatives or exploring other Other Signal Circuits that might match the requirements of their specific applications, findchips.com offers a rich database of parts from STMicroelectronics and other leading manufacturers. This makes it a invaluable tool for comparing and procuring electronic components efficiently and effectively.