MUR860G by onsemi

Overview of MUR860G by onsemi

The MUR860G is a high-performance Power Rectifier, characterized by its ultra-fast recovery and switch-mode capabilities. Designed and manufactured by onsemi, it is primed for applications that demand high efficiency and reliability. With an average forward current of 8 A and a repetitive peak reverse voltage of 600 V, this diode offers robust performance for powering through demanding scenarios. Its forward voltage maximum is capped at 1.5 V, and it boasts an impressively rapid reverse recovery time of 50 Ns. Moreover, the MUR860G can handle forward surge currents up to 100 A, making it exceptionally suitable for applications requiring high surge tolerance.

Its physical packaging is in the TO-220AC 2 Lead form, which is commonly used for high power density and heat dissipation needs. The diode is also RoHS compliant, ensuring adherence to the latest environmental standards regarding hazardous materials. For engineers and procurement specialists focused on integrating environmentally considerate components, the MUR860G stands out not only for its performance but also for its compliance. The component is part of the broader Rectifier Diodes subcategory, known for their role in converting alternating current (AC) to direct current (DC), a fundamental function in power supplies and various electronic circuits.

Industry Applications for MUR860G

The versatile nature of the MUR860G lends itself to a variety of potential industry applications. The following are conceptual illustrations of where this component might be utilized, further emphasizing the necessity for engineering and design teams to verify its adherence to specific application requirements and industry standards:

  • Industrial Automation: The diode’s high forward surge current and ultra-fast recovery time could make it suitable for motor control circuits, power supplies, and other automation equipment that require efficient power conversion and regulation. Its robustness could also contribute to the reliability of automation systems in demanding industrial environments.
  • Consumer Electronics: Devices like power adapters, chargers, and power management modules within consumer electronics could benefit from the MUR860G’s efficiency in power conversion. Its fast recovery time and low leakage current may enhance the performance and energy efficiency of consumer products such as laptops and smartphones.
  • Computing and Data Storage: In the realm of data servers and high-performance computing systems, efficient power supply units (PSUs) are crucial for operational reliability and energy savings. The MUR860G could potentially contribute to the efficiency of these PSUs, thanks to its high voltage and current capabilities, alongside its ultra-fast recovery attribute.
  • Renewable Energy Systems: For applications in solar inverters and wind turbine converters, the MUR860G’s fast switching speed and high voltage tolerance might be advantageous. These systems require components that can handle rapid changes in power levels efficiently, a characteristic that this diode could potentially offer.
  • Telecommunications: In power supply solutions for telecommunications infrastructure, components need to provide consistent, reliable performance. The MUR860G could be considered for its ability to deliver efficient power conversion, contributing to the overall reliability and efficiency of telecom services.

Note that these potential industry applications are only conceptual and require detailed analysis and verification by engineering and design teams to ensure compliance with industry standards and application requirements.

About onsemi

onsemi, formerly known as ON Semiconductor, occupies a significant position in the semiconductor industry, particularly in the development and manufacturing of diodes, including Rectifier Diodes. The company is lauded for its focus on energy efficiency, striving to create electronic components that reduce global energy use. The MUR860G is a testament to onsemi’s commitment to developing components that not only meet the current demands of the electronics industry but also adhere to stringent environmental standards. Onsemi’s portfolio encompasses a wide range of diodes designed for applications that demand high efficiency, reliability, and environmental conformity. Whether it’s power management, signal processing, or protection, onsemi has components that cater to the vast needs of the electronics ecosystem.

Where to Find MUR860G by onsemi

For procurement specialists and engineers seeking to integrate the MUR860G into their designs or systems, finding a reliable source is crucial. Historically, the component has been available at distributors such as Wuhan P&S, Win Source Electronics, Sense Electronic Company Limited, and New Advantage Corporation, among others. However, to get the most current stock levels, pricing, and possible alternative parts, individuals should conduct their research on findchips.com.

By using the search feature on findchips.com, users can access comprehensive information on the MUR860G as well as other Rectifier Diodes. This platform offers the advantage of comparing current offers from diverse distributors, ensuring that users have access to the best possible deal and availability. This detailed approach not only streamlines procurement efforts but also enables better decision-making based on the latest market data.

Compare pricing for MUR860G and other Rectifier Diodes at findchips.com