Overview of 2N7002PS,115 by Nexperia
The 2N7002PS,115 by Nexperia is a dual N-channel Trench MOSFET, encapsulated in a 6-pin TSSOP (SOT363) package. This component is designed for logic level compatibility and is capable of handling a continuous drain current of up to 320 mA. With a drain-source voltage (Vds) of 60V and featuring a low on-resistance of 1.6 Ω at a 10V gate-source voltage, it offers efficient performance in various switching applications. The device operates within an enhanced mode and is built with silicon as the transistor element material.
This MOSFET is distinguished by its dual-gate configuration, separate elements with built-in diodes, and AEC-Q101 compliance, making it suitable for automotive applications. Its maximum operating temperature is specified at 150°C, and it has a moisture sensitivity level of 1, indicating its robustness in varied environmental conditions. Additionally, the transistor is ROHS compliant, affirming its adherence to hazardous substance regulations.
Industry Applications for 2N7002PS,115
The versatile specifications of the 2N7002PS,115 make it suitable for a myriad of applications across different sectors. It is important to note that the following potential applications are conceptual and should be further analyzed by engineering teams to ensure compliance with specific industry standards and requirements.
- Energy and Power Systems: The 2N7002PS,115 could potentially be used in power management modules within energy systems due to its efficient switching capabilities and robust voltage handling. Its AEC-Q101 qualification suggests reliability that could be vital in power supply devices.
- Transportation and Logistics: In electronic control units that require consistent, reliable switching, this MOSFET could provide the necessary durability and performance, significantly in tools used for fleet management and logistics scheduling.
- Renewable Energy: The component’s ability to handle higher voltages and currents lends it use in solar power inverters where switching MOSFETs manage the flow of energy from photovoltaic cells to storage units or the grid.
- Automotive: Given its compliance with automotive standard AEC-Q101, the 2N7002PS,115 is well-suited for applications within vehicular electronics, such as in power control systems, battery management, or even as a part of the electronic drive elements.
These potential applications, however, are only indicative and require thorough evaluation and compliance checks for each specific use case.
About Nexperia
Nexperia, a global leader in the semiconductor industry, specializes in the production of discrete and MOSFET components, and logic & analog ICs. When it comes to Small Signal Field-Effect Transistors, Nexperia provides a diverse range of products that cater to a wide range of applications across different sectors. The 2N7002PS,115, with its dual-gate configuration and Trench MOSFET technology, exemplifies Nexperia’s commitment to innovation and reliability in transistor technology. This dedication is reflected in their compliance with international standards like AEC-Q101, a testament to the company’s focus on quality and performance in automotive-grade components.
Where to Find 2N7002PS,115 by Nexperia
To source the 2N7002PS,115, potential buyers should consider consulting Findchips.com where they can also explore alternatives within the Small Signal Field-Effect Transistors category. Some of the distributors where the part has been historically available include EBV Elektronik, Chip1Stop, Avnet, and Mouser Electronics among others. However, availability and pricing fluctuate, and the latest data should be confirmed on Findchips.com.