AT13-204-2005 by Amphenol Corporation

Overview of AT13-204-2005 by Amphenol Corporation

The AT13-204-2005 is a Connector Accessory, specifically a Sealing Plug designed for ATM-SR Series Connectors. This part is manufactured from thermoplastic and comes in black. The package type for this component is bag, and it is tailored for automotive connectors, ensuring a sealing plug size of 20 suited for 20 AWG wires. The component’s primary function is to provide environmental sealing for connectors, protecting connections from contaminants such as moisture and dust.

As issued by Amphenol Corporation, a notable player in the connector and connector accessory market, this part is RoHS compliant and adheres to REACH guidelines, meaning it is free from certain hazardous materials, making it suitable for use in various environments, including those within the European Union. As of the current writing, the factory lead time for this part is stated as 8 weeks.

Industry Applications for AT13-204-2005

The AT13-204-2005 could find potential applications across numerous industries, given its attributes linked to performance in demanding environments, such as those found in automotive settings. Below are several potential industry applications:

  • Automotive: This sector extensively uses parts like AT13-204-2005 for applications requiring reliable, high-density connections within vehicle electronics, potentially in systems such as infotainment, engine control units, or automotive lighting. The sealing plug can ensure stable and secure connections, essential for the safety and functionality of automotive electronic systems.
  • Industrial Automation: In automated production lines or machinery requiring robust electronic connections, the thermoplastic sealing plug might be used to protect sensor and actuator connectors from industrial contaminants like oils or metal fragments, which could disrupt electronic signals.
  • Aerospace and Defense: Although specific admissions to aerospace certifications like AS9100 were not listed in the part data attributes, the general properties such as reliability in harsh environments suggest potential uses in non-critical avionics or ground-based support equipment that would benefit from such a robust connector accessory.
  • Telecommunications: The component could be employed in the infrastructure for telecommunications where outdoor equipment requires protection against environmental elements to maintain signal integrity and prevent service failures.
  • Note that while these industry applications could potentially benefit from the type, properties or functionality of AT13-204-2005, these scenarios are conceptual and should be further verified by engineering teams specific to each industry.

About Amphenol Corporation

Amphenol Corporation is a leading designer and manufacturer of electrical, electronic, and fiber optic connectors, interconnect systems, and coaxial and specialty cable. Amphenol excels in creating innovative, high-quality interconnect solutions across a wide range of industries. The company plays a significant role in the Assembly Items sector with products like the AT13-204-2005. They offer a diverse array of accessories such as sealing plugs, which are essential for enhancing and securing connections in harsh environments.

Where to Find AT13-204-2005 by Amphenol Corporation

To find the AT13-204-2005, or to explore other Assembly Items that might serve as alternative options, an excellent resource is FindChips.com. Several distributors have historically stocked this part, including New Advantage Corporation, Chip1Stop, Avnet Abacus, TME, TTI, Mouser Electronics, and Avnet Americas. However, prospective buyers should head to FindChips.com to review current stock levels and obtain the latest pricing information.

Compare pricing for AT13-204-2005 and other Assembly Items / Connector Support at findchips.com