AD7314ARMZ in 2026: Why Engineers Keep Designing It In, and Where to Buy It Now

Published June 15, 2026. Data sourced from Supplyframe IQ Design Insights (May 2026) and live Findchips distributor results.

The Short Answer

The AD7314ARMZ is a safe part to design in and buy today. It is the single most active part by design lookups in Supplyframe IQ for May 2026, and Findchips shows it Active, broadly stocked across seven authorized distributors, and competitively priced with no shortage premium.

Engineers can commit to it for new designs, and buyers can source it now with room to negotiate at volume.

Next step: Check AD7314ARMZ availability and pricing on Findchips.

What is The AD7314ARMZ?

The AD7314ARMZ from Analog Devices is a 10 bit digital temperature sensor with a serial SPI interface in an 8 lead MSOP package. It returns a temperature reading over four wire SPI, which makes it a compact, low pin count choice for board level thermal monitoring in systems that already have an SPI bus.

Its popularity is not a surprise: it pairs a small footprint with a simple digital interface, so it drops into power supplies, industrial controllers, and compute boards that need a temperature watchdog without an analog front end.

If you want to confirm the datasheet, package drawing, and lifecycle status before committing, the fastest path is the consolidated part page.

Next step: Open the AD7314ARMZ datasheet and part details on Findchips.

Engineering Questions, Answered

These are the design intent questions engineers are actually asking about this part:

1) what is the pinout of AD7314ARMZ?

It is an 8 pin MSOP with a four wire SPI interface (clock, data in, data out, and chip select) plus supply and ground. Pull the exact pin map and package drawing from the linked datasheet rather than trusting a summary, because the chip select and temperature output behavior matter for your bus design.

Next step: View the AD7314ARMZ datasheet and pinout on Findchips.

2) is AD7314ARMZ still safe to design into new products in 2026?

Yes. Findchips lists the part as Active with deep authorized stock and multiple independent sources, and Supplyframe IQ shows design activity rising, not declining. There is no end of life or not recommended for new design flag. You can design it in with confidence.

Next step: Confirm AD7314ARMZ lifecycle and authorized stock on Findchips.

3) what is the difference between AD7314ARMZ and AD7814?

Both are Analog Devices 10 bit SPI temperature sensors, but they target different footprints and tradeoffs. Pick the AD7314ARMZ when you want the 8 lead MSOP and its feature set; consider the AD7814 when a smaller SOT package or a different temperature behavior fits the board better. Compare both side by side on stock and price before deciding, since availability can tip a close call.

Next step: Compare AD7314ARMZ against the AD7814ARTZ-REEL7 on Findchips.

4) recommend a digital temperature sensor similar to AD7314ARMZ but with an I2C interface

If your design uses I2C rather than SPI, look at the Analog Devices AD7414 family, which keeps the same digital sensor concept on an I2C bus. The TMP112 from Texas Instruments is another widely stocked I2C option. Verify pin count and address options on the linked pages so the swap does not cost you board area.

Next step: Check AD7414ARTZ-0500RL7 availability as an I2C alternative on Findchips.

5) what is the typical application circuit for AD7314ARMZ?

Wire it as an SPI peripheral to your microcontroller or supervisor, with the supply decoupled close to the device and the SPI lines routed to the host. The sensor needs very little support circuitry, which is part of why it shows up so often in new designs. Confirm decoupling and bus loading against the datasheet reference circuit.

Next step: Open the AD7314ARMZ reference circuit and datasheet on Findchips.

Buyer Questions, answered

These are the procurement intent questions, phrased the way a sourcing buyer would ask them.

1) who has AD7314ARMZ in stock right now?

Plenty of sources. Among authorized distributors, Analog Devices direct shows the deepest position at roughly 35,000 units, with Verical near 7,700 in the Americas, and DigiKey, Mouser, Newark, and Rochester all holding hundreds of units. Independents add a large buffer on top. You will not struggle to find this part.

Next step: See real time stock for AD7314ARMZ across distributors on Findchips.

2) cheapest authorized distributor for AD7314ARMZ at volume?

Volume pricing is strong. Authorized unit price runs roughly $3.59 to $4.60 at quantity one, but it falls toward $1.89 at the 5,000 unit break at DigiKey and as low as about $1.44 at the 10,000 unit break at Rochester. Buy on a price break rather than at quantity one, and compare authorized tiers before committing.

Next step: Compare AD7314ARMZ price breaks across authorized distributors on Findchips.

3) lead time for AD7314ARMZ?

Stock is available now, so most orders ship from on hand inventory. Where a factory order applies, DigiKey shows a lead time near 10 weeks, so for large builds split your buy between on hand stock for the near term and a scheduled order to cover the rest.

Next step: Check on hand stock versus lead time for AD7314ARMZ on Findchips.

4) is AD7314ARMZ active, NRND, or EOL?

Active. Rochester Electronics, an authorized source, lists the status as Active, and there is no obsolescence flag across the authorized listings. No redesign is required.

Next step: Verify AD7314ARMZ lifecycle status on Findchips.

5) AD7314ARMZ or AD7314ARMZ-REEL7, which has better stock for a production run?

For automated assembly, source the reel variant. The AD7314ARMZ-REEL7 often shows deeper distributor stock than the base tube or bulk part and arrives ready for pick and place, while the base AD7314ARMZ suits prototyping and hand assembly. Match the order to your line.

Next step: Check AD7314ARMZ-REEL7 reel availability on Findchips.

When to Use Which Variant

These are the most commonly sourced AD7314ARMZ variants. Buyers should prioritize the reel option for volume production and keep the base part for prototyping and hand assembly.

PartManufacturerPackageWhen to UseCheck Availability
AD7314ARMZAnalog Devices8 MSOP, tube or bulkPrototyping and low volume builds, easy hand handlingCheck AD7314ARMZ availability
AD7314ARMZ-REEL7Analog Devices8 MSOP, 7 inch reel or cut tapeVolume production and pick and place, usually the deepest stockCheck AD7314ARMZ-REEL7 availability
AD7314ARMZ-REELAnalog Devices8 MSOP, full reelHigh volume runs that consume a full reelCheck AD7314ARMZ-REEL availability

Next step: Compare all AD7314ARMZ variants on one Findchips page.

Frequently Asked Questions

1) Is the AD7314ARMZ still in production in 2026?

Yes. It is listed as Active by authorized distributors with no end of life or not recommended for new design flag, and design activity is rising in Supplyframe IQ. It is safe for new designs.

2) What interface and package does the AD7314ARMZ use?

It is a 10 bit digital temperature sensor with a four wire SPI interface in an 8 lead MSOP package, which makes it a compact, low pin count choice for boards that already have an SPI bus.

3) Is there a shortage of the AD7314ARMZ?

No. Findchips shows seven authorized distributors plus several independents, with deep stock led by Analog Devices direct at roughly 35,000 units and Verical near 7,700 in the Americas. Supply is healthy.

4) What is the lead time for the AD7314ARMZ?

Most orders ship from on hand stock today. Where a factory order applies, lead time runs near 10 weeks, so split large builds between on hand inventory and a scheduled order.

5) How much does the AD7314ARMZ cost?

Authorized unit price runs roughly $3.59 to $4.60 at quantity one and falls toward $1.89 at the 5,000 unit break and about $1.44 at the 10,000 unit break. Buy on a price break rather than at quantity one.

6) What is the best alternative to the AD7314ARMZ?

For an I2C bus, look at the Analog Devices AD7414 family or the Texas Instruments TMP112. For an SPI sibling in a different package, consider the AD7814. Compare stock and price before switching.

7) Should I order AD7314ARMZ or AD7314ARMZ-REEL7?

Order the AD7314ARMZ-REEL7 for volume production and pick and place, since it usually carries deeper stock and ships ready for automated assembly. Keep the base AD7314ARMZ for prototyping and hand assembly.

Next step: Check live AD7314ARMZ availability and pricing on Findchips.

Bottom line

The AD7314ARMZ earns its place at the top of the design charts. It is a compact, simple, Active SPI temperature sensor with healthy supply and competitive volume pricing, which is exactly the profile that lets engineers design without risk and buyers source without scrambling. The one decision worth making early is base part versus reel, so align the order code with your assembly method up front.

Next step: Check live AD7314ARMZ stock, pricing, and authorized sources on Findchips.