ADXL355BEZ-RL by Analog Devices Inc

Overview of ADXL355BEZ-RL by Analog Devices Inc.

The ADXL355BEZ-RL by Analog Devices Inc. is a low noise, low drift, low power 3-axis accelerometer providing digital output. It is specifically designed to offer precise measurements for applications requiring error-sensitivity and stability, making use of both I2C and SPI communications. Its operational range is configurable at ±2g, ±4g, and ±8g, which makes this accelerometer versatile for a variety of monitoring functions. Packaged in a compact LCC-14 format, it can be integrated into small-form-factor devices.

Operating on a “Lead (Pb)-free” basis yet not in compliance with REACH regulations, this part focuses on eco-friendly operations while maintaining high performance. It features a peak reflow temperature of 260°C for 40 seconds, facilitating its assembly into printed circuit boards without damage. As part of the Other Signal Circuits subcategory, the ADXL355BEZ-RL has been continuously relevant since its introduction to the market in September 2016.

Industry Applications for ADXL355BEZ-RL

The ADXL355BEZ-RL’s capabilities make it potentially suitable for several advanced technological applications. Below, we explore a few industries where this part might be effectively implemented, keeping in mind that these applications should be thoroughly evaluated by engineering teams:

  • Consumer Electronics: The accelerometer could be used in smartphones, fitness trackers, and gaming devices to detect and measure the orientation and motion. The low power requirement and high precision of this accelerometer make it well-suited for these battery-operated devices.
  • Healthcare: In healthcare gadgets like wearable health monitors, the ADXL355BEZ-RL might be used to track patient activity levels or to monitor the stability of the elderly, potentially preventing falls by detecting changes in motion.
  • Industrial Automation: For equipment that requires vibration monitoring to predict maintenance needs, this accelerometer could be integrated to facilitate predictive maintenance algorithms, enhancing operational reliability and efficiency.
  • Transportation and Logistics: In vehicle systems for monitoring stability and control, the accelerometer might contribute to advanced driver-assistance systems (ADAS) by providing critical data for vehicle dynamic controls.

Note: The potential applications listed are for conceptual/illustrative purposes and need verification by industry-specific engineering and design teams.

About Analog Devices Inc.

Analog Devices Inc., widely recognized for its expertise in the design and manufacture of semiconductor products and signal processing technologies, has a robust portfolio in the Other Signal Circuits category. Among these, the ADXL355BEZ-RL represents a focus on integrating high precision and low power consumption, retaining Analog Devices Inc.’s commitment to high-performance solutions across a gamut of electronic applications. Their products often set the benchmark for accuracy, reliability, and durability, providing the foundational components crucial to advancing both industrial and consumer electronics.

Where to Find ADXL355BEZ-RL by Analog Devices Inc.

To obtain the ADXL355BEZ-RL, researching through a reputable distributor aggregator like findchips.com is advisable. This site provides real-time data concerning pricing and availability, particularly essential given the fluctuating inventory levels often experienced in the electronics market. Historically, this part has been stocked by distributors such as Win Source Electronics, LCSC, Richardson RFPD, and Mouser Electronics. By visiting findchips.com, potential buyers can compare current stock availability and pricing not just for ADXL355BEZ-RL, but also for other parts in the Other Signal Circuits category, sourced from Analog Devices Inc. or other manufacturers.

Compare pricing for ADXL355BEZ-RL and other Other Signal Circuits / Signal Circuits at findchips.com