ASMB-MTB0-0B3A2 by Broadcom Limited

Overview of ASMB-MTB0-0B3A2 by Broadcom Limited

The ASMB-MTB0-0B3A2 is a triple color LED that offers colors in red, green, and blue with a diffused lens and a 2.4mm round shape, manufactured by Broadcom Limited. This surface-mount device (SMD) stands out for its common anode, three-element configuration, and is designed to deliver a wide viewing angle of 115 degrees. Each color within the package has been fine-tuned to specific wavelengths: red at 625nm, green at 530nm, and blue at 470nm, ensuring a broad spectrum of visual outputs for various applications. The device boasts luminous intensities of approximately 675mcd for red, 2,675mcd for green, and 535mcd for blue, under a forward current of 20mA for each color channel. Furthermore, its operating temperature ranges from -40°C to a maximum of 100°C, highlighting its adaptability to diverse working conditions. Notably, the LED has achieved RoHS compliance, affirming its environmental friendliness by restricting the use of certain hazardous materials in its manufacture.

Industry Applications for ASMB-MTB0-0B3A2

Potential applications for the ASMB-MTB0-0B3A2 are vast and varied, given its tri-color functionality and the ability to operate across a wide range of temperatures. However, it is important to note that these potential use cases are conceptual and illustrative, requiring further analysis and verification by engineering and design teams to ensure suitability. Here are a few industries where this LED might find application:

  • Automotive: This LED could be used for dashboard lighting, indicator lights, or ambient lighting within vehicles. Its wide viewing angle and bright luminosity make it an ideal choice for both functional and aesthetic applications in automotive design.
  • Consumer Electronics: In devices such as smartphones, tablets, and laptops, the ASMB-MTB0-0B3A2 might serve as status indicators or backlighting for screens and keyboards, providing users with visual feedback through different colors.
  • Lighting Solutions: Given its RGB capabilities, this part could be employed in creating mood lighting, architectural lighting, or stage lighting, where dynamic color changes are required to enhance atmospheres and environments.
  • Signage and Display: Advertising displays, emergency signs, and interactive installations could utilize these LEDs for their ability to command attention through vivid, distinct colors and durable operation over temperature variations.

About Broadcom Limited

Broadcast Limited, renowned for its innovation in the technology sector, has made substantial contributions to the field of optoelectronics, with a particular emphasis on Visible LEDs. The ASMB-MTB0-0B3A2 is among the offerings that underscore Broadcom’s capabilities in providing high-quality, high-performance LED components. Broadcom’s portfolio in optoelectronics spans various applications, leveraging advanced material science, precision engineering, and a deep understanding of the optical properties required in today’s electronic devices. Their products, including various types of visible and invisible light-emitting diodes, cater to a broad spectrum of applications, thereby enabling technology that ranges from consumer electronics to industrial and automotive systems.

Where to Find ASMB-MTB0-0B3A2 by Broadcom Limited

For those looking to procure the ASMB-MTB0-0B3A2, the findchips.com platform offers a centralized location to research availability and pricing. Through Visible LEDs options, users can also explore alternatives to the ASMB-MTB0-0B3A2 that might be offered by Broadcom Limited or other manufacturers. Historically, this part has been available through distributors such as New Advantage Corporation, EBV Elektronik, Ameya Holding Limited, TME, Mouser Electronics, Avnet Americas, DigiKey, and Newark. However, stock levels and availability are subject to change, making it essential for potential buyers to check current listings on findchips.com for the most up-to-date information and best deals.

Compare pricing for ASMB-MTB0-0B3A2 and other Visible LEDs / Optoelectronics at findchips.com