BMP581 Alternatives: Cross-Reference and In-Stock Second Sources

A Findchips engineering spotlight

Engineers searching for BMP581 alternatives usually arrive with the footprint already placed on a PCB and a barometric pressure sensor socket that needs a backup plan. From the outside, the Bosch Sensortec lineup looks like a clean ladder: the BMP280, BMP384, BMP390, BMP580 and BMP581, with each generation quieter and more accurate than the one before. However, if you treat it like a ladder, and simply cross-reference on package and pin count, then you run the risk of sourcing a part that mounts perfectly but never returns a reading.

The reason why is that the BMP5xx generation broke the register map. The BMP580 and BMP581 do not speak the same language as the BMP2xx and BMP3xx parts that came before them, and the Linux kernel treats them as a separate sensor family rather than an extension of the existing driver. That one fact decides which alternatives on your cross-reference list are real and which only appear to be real on a parametric filter.

With this guide, we’ll help you separate the signal from the noise, so you can choose alternates with confidence. 

Our recommendation: Start from the exact Bosch part number your schematic calls out. Search BMP581 listings for live distributor stock on Findchips

What Actually Changed Across Barometric Pressure Sensor Generations

Bosch Sensortec’s BMP581 barometric pressure sensor boasts relative accuracy of roughly plus or minus 0.4 Pa across the 900 to 1,100 hPa band at room temperature, which works out to about 3.3 cm of altitude. Compare that to the parts most designs are using now. The older BMP388 class sits near plus or minus 8 Pa, or roughly half a meter. The even older BMP280 sits near plus or minus 12 Pa, or roughly a meter. That is close to an order of magnitude of improvement in the ability to detect a change in altitude.

Absolute accuracy is the number that does not move nearly as much. Typical absolute accuracy on the BMP581 stays around plus or minus 30 Pa, which is about 2.5 meters, and like every barometric part it still needs a sea level pressure reference to report a true height. Most upgrade arguments skip past this distinction, and it is the whole selection decision. If the application needs to know how high it is, the BMP581 barely pays for itself. If the application needs to know that it moved, it pays for itself several times over.

The rest of the specification supports that same use case. The BMP581 covers 30 to 125 kPa with pressure data resolution of 1/64 Pa, pushes output data rates up to 622 Hz, buffers 32 samples in a FIFO, and offers user programmable low pass and IIR filtering to suppress the noise that doors, windows and airflow inject into an indoor pressure reading. It runs from 1.71 V to 3.6 V in a 2.0 mm square package, so the power rail and the board area rarely drive the decision either way.

Floor level detection, fall detection, drone altitude hold, and HVAC differential work all justify using the BMP5xx generation. Weather logging, indoor air quality and anything that reports an absolute altitude to a user do not.

Next step: Weigh the accuracy tier you actually need against what each part costs today. Compare BMP390 and BMP581 listings on Findchips

Is the BMP581 a Drop-in for Anything Below it?

No, and this is where cross-reference tools mislead. The BMP5xx register map departs significantly from earlier Bosch pressure generations. When support for this family reached the Linux kernel, it arrived as a new set of code paths and a new compatible string rather than a few added constants in the existing BMP280 driver. Firmware written against a BMP280 or a BMP390 does not carry over by changing an address.

That leaves a short and honest alternates list. The BMP580 is the one genuine swap, because it is software and firmware compatible with the BMP581 and differs mainly in measurement precision and price. 

A design that has already been written against the BMP5xx interface can move between the two part numbers by qualifying the accuracy loss, not by touching the driver. Moving down to a BMP390 or a BMP280 is a firmware task with a validation cycle attached, so it belongs in the schedule as engineering work rather than in the bill of materials as a substitute line.

Package dimensions and pin assignments vary across these generations, so confirm the footprint against the current datasheet rather than against a library part inherited from an earlier revision of the board.

Worth considering: If your firmware already targets the BMP5xx interface, the BMP580 is the only true swap. Check BMP580 availability on Findchips

Supplier and Channel Divergence

Second sourcing this socket does not work the way it works for a Schottky rectifier or a small signal diode. There is no industry-type number here, and no competing manufacturer producing a pin and register compatible equivalent. Bosch Sensortec is the source. That means the second sourcing conversation is about channel and about a qualified design in alternate, not about a cross-manufacturer swap.

Two practical consequences follow. First, channel diversification carries more risk mitigation than usual, so it is worth knowing which authorized distributors hold the part and which independent stock is available against an incoming inspection plan. Second, module and breakout labeling deserves scrutiny. 

Boards marketed under a generic BMP58x banner may carry either the BMP580 or the BMP581, and the two differ in exactly the specification most buyers are paying the premium for. It is the same shape of problem as budget boards sold as BME280 that turn out to carry the pressure only BMP280. Confirming the marked part number, not the board description, is the single most useful check on this family.

Next step: Separate authorized stock from independent listings before you commit. Filter live BMP581 distributor results on Findchips

Bosch pressure sensor family comparison

PartMeasuresRelative accuracy classRegister familyBest fit
BMP280Pressure, temperatureAbout 1 mBMP2xxCost-driven and legacy designs, deep stock
BME280Pressure, temperature, humidityAbout 1 mBMP2xxEnvironmental sensing where humidity is required
BMP384Pressure, temperatureBMP38x classBMP3xxExposure to liquids and chemicals, gel-filled construction
BMP390Pressure, temperatureAbout 0.5 mBMP3xxMainstream altitude tracking, mature driver support
BMP580Pressure, temperatureBMP5xx classBMP5xxCost-aware BMP5xx designs, firmware compatible with BMP581
BMP581Pressure, temperatureAbout 3.3 cmBMP5xxPrecision relative altimetry, wearables and drones

Read the register family column before the accuracy column. It is the one that determines whether a candidate is a purchasing decision or an engineering project.

Next step: Price the whole family in one view before you lock the socket. Search Bosch pressure sensor listings on Findchips

Where the Motion Sensor Pairs in

Precision pressure rarely ships alone. The applications that justify a BMP581, like altitude hold on a small drone and activity tracking on a wearable, almost always place it next to a six-axis motion sensor so that altitude and orientation arrive on the same timeline. That pairing is why the pressure socket and the motion socket tend to get specified in the same design review.

The sourcing risk is not evenly distributed across those two sockets, though. Barometric parts have generally held reasonable availability, while the popular six-axis parts have been the ones carrying long authorized lead times and pushing designs toward a qualified alternate. If your design pairs the two, the motion sensor is usually where the schedule risk lives.

Next step: See how the motion socket changes the sourcing picture in our ESP32-S3 motion node reference design and sourcing guide

Frequently asked questions

Is the BMP581 a drop-in replacement for the BMP390?

No. The BMP5xx generation uses a different register map from the BMP3xx parts, so firmware written for a BMP390 will not communicate with a BMP581 without driver work. Package and land pattern should be verified separately.

What is the closest alternate to the BMP581?

The BMP580. It is software and firmware compatible with the BMP581 and differs mainly in measurement precision and price, which makes it the only candidate that behaves as a true substitution rather than a redesign.

Does the BMP581 improve absolute altitude accuracy?

Only modestly. Typical absolute accuracy stays around plus or minus 30 Pa, or about 2.5 meters. The large improvement is in relative accuracy, roughly plus or minus 0.4 Pa, which is what makes the part suitable for detecting small changes in height rather than reporting a true elevation.

Why do breakout boards labeled BMP58x behave differently from each other?

Because a generic BMP58x label can cover either the BMP580 or the BMP581, and the two differ in accuracy and cost. Confirm the marked part number on the sensor rather than trusting the board description.

The bottom line

The BMP581 is not an upgrade you drop into an existing pressure socket. It is a new generation with its own register map, and the only alternate that behaves like a substitution is its immediate sibling. Everything below it in the family is a firmware project wearing the costume of a cross reference.

That makes the selection decision unusually clean. Decide first whether the design needs relative resolution or absolute altitude, because that answer alone eliminates most of the family. Then determine whether the firmware is already written against the BMP5xx interface, because that factor determines whether your second source is a purchase order or a sprint. Everything after that is a question of who has stock today.

Before you go: Start the cross reference with live availability in front of you. Compare BMP581 and BMP580 pricing and stock on Findchips