Buck Converter Alternatives: Why Pin Compatibility Does Not Mean Drop-In Compatibility 

When a point-of-load rail goes on allocation, the fastest fix is to conduct a parametric search. Filter the search on input range, output current, and package, then sort by stock, and pick the part that lands on the same footprint. This way, the board does not change and the build moves ahead. 

However, this workflow produces buck converter alternatives that fit the footprint but behave differently once powered. Texas Instruments’ TPS54302 is a useful example. The device is a 4.5 V to 28 V input, 3 A synchronous buck converter in a SOT-23 six-pin package, and dozens of parts from at least six manufacturers share that outline. Despite this high-level compatibility, very few of these parts are interchangeable with the TPS54302. 

Next step: Check current distributor stock and lead times for the TPS54302 before committing to a substitution path. 

What Makes One Buck Converter a Real Alternative to Another 

A buck converter is a switched-mode step-down regulator, and the category is enormous. Narrowing it to parts that could physically replace a specific device on an existing board means answering three separate questions, and most cross-reference tools only answer the first. 

1) Package outline. Does the substitute have the same land pattern? SOT-23-6, TSOT-23-6, SOT-563, and SOT-583 are all small six- or eight-pin outlines, but they do not have the same land pattern. Texas Instruments’ recommended alternate for the TPS54302 with a higher switching frequency and lower quiescent current is the TPS62933, which is a 3.8 V to 30 V, 3 A part in a SOT-583 package. That requires a board revision, not a BOM swap. 

2) Pin assignment. Does the substitute use the same signal on the same pin? Sharing an outline does not mean sharing a pinout. The TPS54302 uses VIN, EN, GND, BOOT, FB, and SW across its six pins. A six-pin buck converter from another manufacturer may assign those same six functions in a different order, which turns a footprint match into a short circuit. 

3) Electrical behavior. Does the substitute regulate the same way? This is where most substitutions actually fail, and it is the layer nobody checks because it is invisible in a parametric filter. 

Next step: Compare availability across the TPS62933 supply base if a board revision is already on the table. 

The Four Parameters That Determine Whether a Substitution Works 

Once package and pinout are clear, four electrical characteristics determine whether the substitute will actually work in the same circuit with the same external components: 

1) Switching frequency. The TPS54302 runs at a fixed 400 kHz. Frequency sets the inductor value for a given ripple current, so a substitute at 1.2 MHz or 2 MHz will run a very different ripple through the inductor you already have on the board. Parts with an adjustable frequency range, such as the 200 kHz to 2.2 MHz devices in the TPS629xx family, give you a way out, but only if you have a spare resistor position to set them. 

2) Control architecture. The TPS54302 uses peak current mode control. The TPS563257 employs voltage mode control with pulse width modulation. Texas Instruments’ LM5013 buck converter uses constant on-time operation. These are three different loop behaviors under load transients, and because compensation is internal on all of them, you cannot retune the loop to match. Control architecture is rarely exposed as a filter field, and it is the single most common reason a footprint-compatible substitute produces different transient response on the bench. 

3) Light load behavior. The TPS54302 implements Advanced Eco-mode pulse skipping to raise light-load efficiency. Texas Instruments also lists an equivalent part that runs in forced continuous conduction mode instead. Both are legitimate designs, but they behave differently below a few hundred milliamps. Pulse skipping raises efficiency and introduces low-frequency output ripple. Forced continuous conduction holds ripple flat and burns more current. If the rail feeds an ADC reference or an RF section, that difference is a design change, not a preference. 

4) EMI features. The TPS54302 includes frequency spread spectrum specifically to reduce EMI. A substitute without spread spectrum concentrates its emissions at the fundamental and its harmonics. If the original design passed radiated emissions with spread spectrum enabled, a substitution that removes it puts you back in the EMC test chamber. 

Next step: Review the AP63301 supply base and package options when evaluating a cross-manufacturer alternate. 

Comparing Candidate Alternates 

The table below shows how quickly nominally similar parts diverge. Every device listed is a synchronous buck converter in a small integrated package, and several are surfaced as alternates to each other by parametric search. 

Part Input range Max output Switching frequency Package 
TPS54302 4.5 V to 28 V 3 A Fixed 400 kHz SOT-23-6 
TPS62933 3.8 V to 30 V 3 A 200 kHz to 2.2 MHz SOT-583 
TPS62932 3.8 V to 30 V 2 A 200 kHz to 2.2 MHz SOT-583 
TPS563257 3 V to 17 V 3 A 1.2 MHz SOT-563 
AP63301 3.8 V to 32 V 5.2 A Up to 550 kHz TSOT-26 
LT8609 3 V to 42 V 3 A 2 MHz MSOP 

Read across any row and the differences compound. The TPS563257 covers a similar output current in a package similar in size to the TPS54302, but its input ceiling is 17 V rather than 28 V and it switches three times faster.  

Diodes Inc.’s AP63301 carries more current and adds AEC-Q100 qualification, which matters if the design is heading into an automotive program, but its input range and frequency both differ.  

None of these is a drop-in replacement for the TPS54302, but all of them will appear in a loosely filtered search. 

Next step: Pull live distributor coverage for the TPS563257 alongside the incumbent part to compare supply depth. 

Building a Defensible Cross-Reference 

The sequence that holds up under review is narrower than the one parametric search encourages. Start from the rail requirement rather than the incumbent part. Confirm the land pattern from the mechanical drawing rather than the package name, then confirm the pinout function by function. 

Check the four electrical parameters above against the rail specification. If switching frequency changes, recalculate the inductor. If light-load behavior changes, confirm the minimum load. If EMI features change, plan for retest. 

Finally, check supply depth across the whole candidate set rather than qualifying a single alternate. A second source available from one distributor has not solved the problem that caused the substitution. 

Next step: Check multi distributor availability for the MP2143 as part of a full candidate set review. 

Frequently Asked Questions 

Is a buck converter with the same package and pinout always a drop-in replacement? 

No. Package outline and pin assignment are only the first two of three compatibility layers. Switching frequency, control architecture, light-load behavior, and EMI features all affect whether the substitute works with the existing external components, and none of them are visible in a package or pinout match. 

Why can’t I just retune the compensation network on a substitute part? 

Small integrated buck converters such as the TPS54302 use internal loop compensation, which means the compensation network is inside the silicon and not accessible from the board. There is no external component to adjust, so a substitute with a different loop response must be accepted as designed or rejected. 

Does changing switching frequency mean I have to change the inductor? 

Usually yes. Switching frequency sets the inductor value required for a given ripple current, so a substitute that switches at a significantly different frequency will produce different ripple through the existing inductor. Recalculate the inductor value against the new frequency before assuming the existing part is adequate. 

What is the difference between pulse skipping and forced continuous conduction at light load? 

Pulse skipping, such as the Advanced Eco-mode implementation in the TPS54302, raises efficiency at light load and introduces low-frequency output ripple. Forced continuous conduction keeps ripple flat and consumes more quiescent current. The choice matters when the rail feeds a noise-sensitive load such as an ADC reference or an RF section. 

Next step: Compare current sourcing options for the LT8609 when a wider input range is required. 

Conclusion 

Buck converter alternatives tend to fail in a specific and predictable way. The footprint matches, the parametric summary looks close, and the difference shows up on the bench as ripple, transient response, or a failed emissions scan. 

The solution is to treat the footprint match as the beginning of the evaluation rather than the end of it. Specify the rail, verify all three compatibility layers, and check supply depth across the full candidate set before qualifying any single part. 

Next step: Start a cross manufacturer buck converter search to see live availability across the category before narrowing your candidate list.