DA14531-00000FX2 by Renesas Electronics Corporation

Overview of DA14531-00000FX2 by Renesas Electronics Corporation

The DA14531-00000FX2, part of the SmartBond™ series from Renesas Electronics Corporation, is an ultra-low power Bluetooth® 5.1 System-on-Chip (SoC) that comes in a FCGQFN package with a supply format of 4000 per tape & reel. This particular SoC integrates an ARM Cortex M0+ processor, positioning it as an efficient solution for developers looking to incorporate Bluetooth 5.1 connectivity into their applications. This part is categorized under Other uPs/uCs/Peripheral ICs within the broader Microcontrollers and Processors category.

Some additional notable characteristics of the DA14531-00000FX2 include being Pb-free and RoHS compliant, ensuring adherence to global environmental and safety standards. The part is listed as having an active part life cycle status by the supplier, Renesas Electronics Corp, indicating ongoing production and support. The package’s terminal finish is Nickel/Palladium/Gold (Ni/Pd/Au), and it boasts a Moisture Sensitivity Level (MSL) of 1, which denotes a high level of resilience against moisture. With a factory lead time of 18 weeks, as of the current writing, planning for procurement should consider this timeframe. The SoC is also characterized by its reach compliance and bears the JESD-609 Code e4.

Industry Applications for DA14531-00000FX2

The DA14531-00000FX2’s capabilities make it a potentially suitable component for various applications across a spectrum of industries. However, it is critical to remember that these potential applications are conceptual and should be thoroughly analyzed by engineering and design teams to ensure adherence to industry standards and specific application requirements. Here are a few industries where the DA14531-00000FX2 might find relevance:

  • Consumer Electronics: Its ultra-low power consumption and Bluetooth 5.1 capability could make the DA14531-00000FX2 an ideal component for small, energy-efficient wearable devices such as fitness trackers and smartwatches, potentially enhancing connectivity and extending battery life.
  • Smart Cities: In smart city infrastructure, the DA14531-00000FX2 might be used in sensor networks for monitoring environmental conditions, traffic flow, or public lighting systems, leveraging its low energy Bluetooth SoC for long-term, reliable wireless data transmission.
  • Healthcare: The device’s high moisture sensitivity resistance and low power draw could make it suitable for portable health monitoring devices, possibly enabling continuous patient monitoring without frequent recharging.
  • Industrial Automation: The DA14531-00000FX2 could potentially be used in the development of connected industrial sensors and actuators, offering a blend of real-time data communication and low-energy operation, crucial for maintaining efficient production lines.
  • Internet of Things (IoT): Given its Bluetooth SoC characteristics, the DA14531-00000FX2 is potentially an excellent fit for a range of IoT devices, facilitating the development of energy-efficient, connected home automation systems, and other IoT solutions.

Note that for applications within the automotive or medical imaging sectors, or for military or defense applications, specific compliance standards such as AEC-Q100 or MIL-SPEC must be verified against the part’s specifications and certifications.

About Renesas Electronics Corporation

Renesas Electronics Corporation is a formidable player in the microcontrollers and processors domain, especially known for its contributions to the Other uPs/uCs/Peripheral ICs sub-category. The company’s dedication to innovation is evident in its diverse portfolio, which includes the DA14531-00000FX2 amongst other remarkable components like the wider SmartBond™ series. Renesas prioritizes aspects such as power efficiency, connectivity, and comprehensive solution platforms, catering to the evolving needs of the electronics industry. Their products are integral to advancing microcontroller and processor technology, pushing the boundaries of what’s possible in the design and development of new and existing applications across various sectors.

Where to Find DA14531-00000FX2 by Renesas Electronics Corporation

To source the DA14531-00000FX2 and to explore other potential Other uPs/uCs/Peripheral ICs that could meet your project requirements, FindChips.com is an invaluable resource. This platform enables you to compare pricing, availability, and specifications for the DA14531-00000FX2 across multiple distributors. Historically, distributors like Avnet Asia, Avnet Americas, Renesas Electronics America, Mouser Electronics, Avnet Silica, DigiKey, and Farnell have carried this part. However, for the most current stock levels, pricing information, and to explore alternative options provided by both Renesas Electronics Corporation and other manufacturers, we recommend conducting your research via FindChips.com.

Compare pricing for DA14531-00000FX2 and other Other uPs/uCs/Peripheral ICs / Microcontrollers and Processors at findchips.com