Overview of DLW44SM101SK2L by Murata Manufacturing Co Ltd.
The DLW44SM101SK2L is a common mode choke designed specifically for use as a Data Line Filter. It features a compact size of 4mm x 4mm x 1.4mm, making it suitable for surface mount applications. This component offers a rated current of 3.1 A and an output impedance of 100 Ohm, which is critical for maintaining signal integrity and reducing electromagnetic interference (EMI) in electronic circuits.
Manufactured by Murata Manufacturing Co Ltd, the DLW44SM101SK2L adheres to the RoHS directives, ensuring compliance with environmental standards. It has an insulation resistance of a minimum of 10 MΩ, making it reliable for various applications. The filter operates effectively within a temperature range of -40 °C to 105 °C and has a DC resistance maximum of 0.0224 Ω. The packaging method is tape and reel, facilitating easy integration into automated assembly processes.
As of the current writing, this part is classified as active in the market, which indicates that it is still being produced and supported by the manufacturer. These specifications make it an important component in the arsenal of electronic parts utilized by engineers and designers in various applications.
Industry Applications for DLW44SM101SK2L
The DLW44SM101SK2L could find potential applications across various industries, particularly those that require effective filtering of electrical noise or interference in data transmission. Below are a few illustrative examples:
- Telecommunications: This part might be used in base stations or other telecommunications devices where signal integrity is critical. The 100 Ohm output impedance could assist in matching impedance in high-speed data lines, potentially helping to minimize signal reflections and loss.
- Education and Research: In academic settings, the DLW44SM101SK2L might be implemented in experimental setups, such as data acquisition systems. As researchers develop new technologies that require reliable data transmission, the choke could support improved communication systems.
- Consumer Electronics: The compact design of the DLW44SM101SK2L could make it suitable for integration into small form-factor devices like tablets or smartphones. It might assist in managing the effects of EMI, ensuring stable and clear communication within the device’s circuitry.
- Industrial Automation: In industrial settings, this part could be utilized in various control systems, where it might help maintain data integrity across sensor networks. The ability to handle a rated current of 3.1 A could make it viable for use in equipment that requires considerable power while still managing signal noise.
It is important to note that these potential industry applications are only conceptual and require analysis and verification by engineering and design teams for adherence to industry standards and specific application requirements. Other similar parts in this category might also serve these applications, highlighting the importance of careful selection when designing circuits.
About Murata Manufacturing Co Ltd.
Murata Manufacturing Co Ltd. is a well-established manufacturer in the electronic components industry, particularly recognized for its development of passive components, including Data Line Filters such as the DLW44SM101SK2L. The company places a strong emphasis on innovation and quality, producing a wide array of filtering solutions that cater to the needs of various industries. Their solutions often focus on optimizing performance while adhering to international safety and environmental standards.
Murata’s portfolio includes various types of filters, which are crucial for managing noise in electronic signals. Other components that are similar to the DLW44SM101SK2L might include different choke configurations and data line filters aimed at specific applications, showcasing their versatility and commitment to meeting diverse customer needs.
Where to Find DLW44SM101SK2L by Murata Manufacturing Co Ltd
- Avnet Abacus
- TME
- TTI
- Future Electronics
- Mouser Electronics
- Avnet Americas
- DigiKey
Note that availability may vary, so it is essential to consult findchips.com for the most current stock levels and pricing information before making a purchase.