Four Trends to Watch in 2026 Electronic Component Sourcing

By Jonathan Cassell

With the new year upon us, Supplyframe has identified four critical trends that may shape electronic component procurement conditions in 2026. By monitoring and preparing strategies to deal with these developments, buyers can gain a competitive advantage over the next 12 months.

Supply chain risk elevates in 2026 

Traditionally, the overriding concern in the electronics procurement sector has been cost. However, in recent years, risk has emerged as an increasingly critical issue facing electronic component buyers. In 2026, risk management is set to become the paramount consideration in the supply chain, as international tensions escalate.

The imposition of U.S. tariffs has spurred concerns over supply-chain risk. Beyond simply raising prices, the frequently changing tariff situation has added major uncertainty to the sourcing outlook, making planning difficult.

Moreover, the tariffs and rising geopolitical instability have scrambled the customary order in the international trade system, with the U.S. increasingly at odds with countries that were formerly its closest partners. In parallel with the uncertain trade conditions, international relations have entered a new phase of unpredictability.

All these factors have thrown the supply chain into chaos, with long-held trade relationships now cast into doubt.

Under these circumstances, the China-plus-one strategy is no longer a satisfactory solution to today’s supply challenges. With the current state of trade disorder, the next supply chain disruption could originate from anywhere in the world and affect any component or raw material.

As a result, buyers should adopt more flexible strategies, sourcing components from a wider array of countries, including Vietnam, Thailand, and Mexico. By taking this approach, buyers can potentially mitigate the impact of tariff-related trade disruptions and maintain supply assurance.

Cost remains critical

While risk mitigation is the top concern, cost is also a major consideration in 2026.

Raw material costs have surged in recent times, due to trade tensions and growing economic uncertainty. Pricing for precious metals has surged as central banks and individual investors move to lower-risk investments.

Meanwhile, copper prices are soaring due to demand- and supply-side factors as well as trade issues that are all impacting the supply chain simultaneously. Rare earth pricing has also risen dramatically due to export restrictions instituted by China. Costs for cobalt commonly used in batteries for portable electronic devices rose sharply in 2025 as the Democratic Republic of Congo ceased exports.

Moreover, supply-chain decoupling and the geographic diversification of supply can trigger further price increases. The establishment of new factories outside of China and the addition of new country-of-origin (COO) requirements stand to increase capital expenditures for suppliers, driving up costs.

Buyers should closely monitor raw material costs and find new sources of supply that have less exposure to inflationary factors. They should also aim to find substitute materials wherever possible.

Shortages return

After suffering crippling shortages during the Covid era, the specter of a new round of scarcity is haunting electronic component buyers.

The AI boom has already led to constrained supplies of GPUs and certain types of high-performance memory used in AI servers. However, the price impact is beginning to spread to other electronic product classes.

Other types of memory are increasingly experiencing constraints as suppliers shift production away from older devices and toward AI-oriented parts. Tantalum capacitors used in servers are experiencing extended lead times. Supplies of discretes used for power management are also being snapped up by data centers.

If the AI boom persists in 2026, these shortages could bleed over to even more components. Under these circumstances, procurement management organizations are advised to restart the semiconductor purchasing task forces they originally established in the early 2020s to manage the shortage situation. These operations should keep a close eye on lead times to gauge the severity of shortages and formulate strategies to deal with shortfalls.

The probability of an AI bust increases

Most signs point to the continuation of the AI boom in 2026, with companies issuing rosy outlooks and capital expenditure outlooks soaring. However, the chorus of concerns about the longevity of the AI phenomenon is growing louder. Observers have pointed to everything from a lack of return on investment to the increasingly circular nature of AI investments as signs that the bubble may soon pop.

Whether or not such a crash comes to pass in 2026, buyers should be prepared for a rapid shift in supply conditions, similar to what occurred during the dot-com bust in 2000. The onset of the dot-com bust transformed the electronics market, with order cancellations spurring a rapid drop in demand for a vast range of components, bringing a rapid end to a period of acute shortages.

Buyers should keep a close eye out for any signs of softening in pricing and lead times for GPUs, memory, high-end networking, power, and data-center passives. These developments could signal the end of AI-driven shortages.

Buyers will need to react rapidly, renegotiating deals and trimming orders to limit inventory overhang and obtain more favorable pricing and lead time terms.

Jonathan Cassell is the lead analyst for Supplyframe Commodity IQ