IRF1010EZPBF by Infineon Technologies AG

Overview of IRF1010EZPBF by Infineon Technologies AG

The IRF1010EZPBF by Infineon Technologies AG is a N-channel Power Field-Effect Transistor (FET) designed for high-efficiency power management and switching applications. Characterized by a drain current of 75A, a drain-source voltage of 60V, and a drain-source on-resistance of just 0.0085Ω, this component offers exceptional performance for its class. It is built in a TO-220AB package which is a through-hole, flange mount configuration that facilitates ease in mounting and heat dissipation.

In terms of structural design, the IRF1010EZPBF is encapsulated in a plastic/epoxy material which supports its robustness in various operating environments. It operates in enhancement mode with a maximum operating temperature of 175°C, providing a suitable choice for thermal management in demanding applications. Additionally, the device features built-in diode configuration and avalanche-rated capabilities, making it resilient to voltage spikes and enhancing its reliability in power switching circuits.

Industry Applications for IRF1010EZPBF

The IRF1010EZPBF’s robust performance characteristics make it adaptable for a variety of industry applications, although these suggestions remain conceptual and should be validated by engineering teams against specific requirements. The following applications could potentially benefit from this transistor:

  • Industrial Automation: The high current and voltage capabilities might make the IRF1010EZPBF ideal for driving high-power motors and actuators commonly found in automated machinery.
  • Consumer Electronics: Devices such as power supplies for computers and TV sets could utilize this MOSFET for efficient power regulation, given its ultra-low on-resistance which improves overall energy efficiency.
  • Telecommunications: Base station power management modules might integrate this component to handle high current operations reliably, potentially enhancing signal transmission reliability and system longevity.
  • Computing and Data Storage: The thermal and switching characteristics of the IRF1010EZPBF could also make it a strong candidate for managing power in servers and storage systems, where maintaining electrical efficiency and heat dissipation is critical.
  • Renewable Energy Systems: In applications like solar inverters, which require robust switching capabilities, the avalanche-rated feature of this transistor could provide added reliability against unpredictable voltage fluctuations.

It’s crucial to note that these applications should be evaluated for engineering feasibility and compliance with industry standards before implementation.

About Infineon Technologies AG

Infineon Technologies AG is a prominent leader in semiconductor solutions, focusing broadly on automotive, industrial, and IoT sectors. Within the realm of transistors, particularly within Power Field-Effect Transistors, Infineon is known for its innovative approaches that integrate advanced technology to meet the rigorous demands of modern electronic applications.

The production of components like the IRF1010EZPBF underscores Infineon’s commitment to delivering high-reliability products capable of handling significant power densities and efficiency. They often incorporate features such as avalanche ruggedness and low on-resistance, enhancing their appeal across various high-stakes applications. Infineon continues to develop technologies within the FET domain, pushing the boundaries in terms of what can be achieved with semiconductor materials.

Where to Find IRF1010EZPBF by Infineon Technologies AG

To purchase the IRF1010EZPBF, one should visit findchips.com where you can access current stock levels and pricing from various distributors. Previously, this part has been available from distributors such as New Advantage Corporation, EBV Elektronik, TME, and DigiKey. By using findchips.com, potential buyers can explore available inventory from these and other distributors to make an informed purchasing decision. For alternative parts, one could also refer to Power Field-Effect Transistors to explore other options from Infineon or different manufacturers.

Compare pricing for IRF1010EZPBF and other Power Field-Effect Transistors / Transistors at findchips.com