Overview of IS82C54-10Z96 by Renesas Electronics Corporation
The IS82C54-10Z96 is a CMOS programmable interval timer that operates at a maximum frequency of 10 MHz. This integrated circuit, packaged in a 28-pin Plastic Leaded Chip Carrier (PLCC), offers a versatile solution for various timing applications. Key features of this part include a supply voltage range from 4.5 V to 5.5 V, making it suitable for standard logic power supplies. The operating temperature range is rated from -40 °C to 85 °C, classifying this component for industrial applications.
With three independent timers, the IS82C54-10Z96 allows for parallel processing and direct addressability, with an external data bus width of 8-bits. This configuration provides flexibility in programming and ease of integration into existing systems. The part is designed to be compliant with lead-free and RoHS standards, ensuring adherence to environmental regulations.
As of the current writing, the factory lead time for this component is approximately 24 weeks. This data is essential for planners who need to account for lead times in their production schedules.
Industry Applications for IS82C54-10Z96
This component could potentially find applications across various industries. Below are some illustrative examples of how the IS82C54-10Z96 might be utilized in different sectors. It is important to note that these applications are conceptual and require thorough analysis and verification by engineering and design teams for adherence to industry standards and specific application requirements.
- Industrial Automation: In industrial settings, the IS82C54-10Z96 might be used in programmable logic controllers (PLCs) for managing timing functions in machinery. Its ability to work with multiple timers could support complex operational tasks, possibly improving efficiency in assembly lines or automation systems.
- Renewable Energy: The timer could potentially serve a role in monitoring and controlling systems within renewable energy installations, such as solar inverters. It might assist in scheduling operations or managing the timing of power delivery based on solar input, which could optimize energy usage.
- Robotics and Drones: Within robotics, the IS82C54-10Z96 could be integrated into control systems to manage timing for sensor data sampling and motor operations. This might enhance the responsiveness of robots or drones, which often rely on precise timing for navigation and task execution.
- Consumer Electronics: This programmable timer might be utilized in consumer electronics where timing is critical, such as in digital clocks or timers within kitchen appliances. Its compact size and programmable nature could make it suitable for small electronic devices that require accurate timing.
- Telecommunications: The IS82C54-10Z96 could potentially be applied in telecommunications equipment for managing synchronization tasks. Its ability to operate efficiently under varying temperature conditions might be beneficial for devices deployed in diverse environments.
About Renesas Electronics Corporation
Renesas Electronics Corporation is a leading provider of semiconductor solutions that are focused on microcontrollers and processors, along with other electronic components such as the IS82C54-10Z96. The company has a strong presence in the realm of timers and real-time clock (RTC) solutions, providing a range of products designed to meet the diverse needs of industries such as automotive, industrial automation, and consumer electronics.
In addition to the IS82C54-10Z96, Renesas offers a variety of similar programmable timers that could be suitable for applications requiring timing precision and reliability. Their portfolio demonstrates a commitment to developing products that not only meet technical requirements but also adhere to environmental standards.
Research Price and Stock for IS82C54-10Z96 by Renesas Electronics Corporation on Findchips.com
For those interested in the IS82C54-10Z96, it is advisable to research stock and pricing through Findchips. This platform can provide insights into current availability and price comparisons across various distributors. Historical distributors where this part has been available include:
- Avnet Silica
- Future Electronics
- Mouser Electronics
- Avnet Americas
- DigiKey
- Newark
However, please visit Findchips for the most accurate and up-to-date information regarding stock levels and pricing for the IS82C54-10Z96. The site can also help identify alternate parts within the Timers or RTCs subcategory that might be offered by Renesas Electronics Corporation or other manufacturers.