JANTX2N6788 by Infineon Technologies AG

Overview of JANTX2N6788 by Infineon Technologies AG

The JANTX2N6788 represents a N-Channel Power Field-Effect Transistor (FET) designed for high-performance applications within various electronic systems. It features a maximum drain current of 6 A and operates at a maximum voltage of 100 V, making it suitable for several applications that require reliable switching and amplification. The device has a drain-source on-resistance of 0.35 ohms, which can contribute to reduced power losses during operation. With a power dissipation rating of 20 W, the JANTX2N6788 can manage significant power levels efficiently.

This component is housed in a TO-205AF package which is hermetically sealed and designed in a modified TO-39 form factor that incorporates three terminals. The package’s metal construction offers greater durability and a higher level of protection against environmental factors, thus ensuring the longevity and stability of the transistor in operational settings.

Notably, the JANTX2N6788 is classified as avalanche rated with an energy rating of 0.242 mJ, allowing it to withstand transient voltage spikes without failure. The enhancement-mode operating characteristics of this transistor allow for improved conduction and efficiency in active circuits. The maximum operating temperature is rated at 150 °C, providing flexibility for use in high-temperature environments.

At the time of this writing, the factory lead time is noted to be approximately 4 weeks, which is beneficial for planning procurement and inventory management.

Industry Applications for JANTX2N6788

The versatility of the JANTX2N6788 makes it potentially applicable in various industries, including:

  • Consumer Electronics: This transistor might be employed in devices such as televisions, audio amplifiers, or power supplies, where efficient switching is crucial. The low on-resistance helps in minimizing heat generation during operation, which could enhance the performance and reliability of consumer devices.
  • Industrial Automation: In control systems or automation equipment, this transistor might be used for driving motors or actuators. The ability to handle higher currents could present opportunities for its use in programmable logic controllers (PLCs) or robotics, where switching capabilities are essential.
  • Energy and Power Systems: The JANTX2N6788 could find applications in power management systems, such as converters and inverters. Its avalanche rating might provide additional safety and reliability in scenarios involving power spikes, which is critical in renewable energy systems such as solar inverters.
  • Motor Control Systems: In applications requiring precise motor control, this transistor might be utilized in H-bridge circuits or other configurations. Its ratings align with the demands of motor control, where rapid switching and current handling are important to prevent thermal issues.

These potential industry applications are purely conceptual and illustrative. Engineering and design teams should conduct thorough analysis and verification to ensure adherence to industry standards and specific application requirements.

About Infineon Technologies AG

Infineon Technologies AG is a global semiconductor manufacturer known for its extensive portfolio of products designed for various electronic applications. Within the realm of transistors, the company offers a range of high-performance devices, including the JANTX2N6788. Infineon’s focus on innovation in Power Field-Effect Transistors has led to the development of components that provide efficient power conversion and management solutions.

The company’s transistors are often used in industries ranging from automotive to industrial automation, with an emphasis on reliability and efficiency. Similar parts may include various configurations and ratings under their MOSFET offerings, which meet the diverse needs of engineers and designers seeking effective solutions for their electronic designs.

Where to Find JANTX2N6788 by Infineon Technologies AG

For those interested in procuring the JANTX2N6788, it is recommended to research purchasing options on findchips.com. This platform provides comprehensive information on stock levels and current pricing. Users can also explore alternative options among Power Field-Effect Transistors from Infineon Technologies AG and other manufacturers that may fit specific application needs.

Historically, distributors such as Future Electronics have offered the JANTX2N6788. However, it is advisable to check findchips.com for the latest availability and pricing, as stock levels can fluctuate based on market demand and supply chain factors.

Compare pricing for JANTX2N6788 and other Power Field-Effect Transistors / Transistors at findchips.com