Overview of LBEE5PL2DL-921 by Murata Manufacturing Co Ltd.
The LBEE5PL2DL-921 is a high-performance, shielded small Wi-Fi 11a/b/g/n/ac/ax + Bluetooth 5.3 module designed for a range of telecommunication applications. This part is classified under the Other Telecom ICs subcategory of Telecommunication Circuits, indicating its specialized role in the field of wireless communication technology. As a multiprotocol module, it supports both Wi-Fi and Bluetooth protocols, which makes it extremely versatile for integrating wireless communication capabilities into electronic devices.
Murata Manufacturing Co. Ltd, the manufacturer of this component, ensures that the module is compliant with the latest environmental standards, as it is designated with a RoHS (Restriction of Hazardous Substances) Code of “Yes”. Its active lifecycle status indicates ongoing manufacturer support and availability. The part also has a moisture sensitivity level of 3, which delineates handling requirements for avoidance of moisture-induced damage during the assembly process. The typical factory lead time for this component is 28 weeks, as of the current writing, suggesting planning for procurement schedules.
Industry Applications for LBEE5PL2DL-921
The LBEE5PL2DL-921 can be potentially utilized across various industries where wireless communication is critical. Here are some illustrative use cases:
- Consumer Electronics: Devices such as smartphones, tablets, and smart home products could potentially incorporate this module to enable or enhance their Wi-Fi and Bluetooth functionalities. The compatibility with multiple Wi-Fi standards and Bluetooth 5.3 is particularly beneficial for ensuring devices can operate in diverse connectivity environments.
- Industrial Automation: Wireless controllers and sensors in manufacturing plants might use the LBEE5PL2DL-921 to reliably communicate over both Wi-Fi and Bluetooth networks. This could potentially improve the flexibility and scalability of automation systems.
- Internet of Things (IoT): In IoT ecosystems, this component could potentially be utilized in connected devices ranging from consumer IoT products to industrial IoT applications, enabling them to connect seamlessly with other devices and networks thereby enhancing interoperability.
- Medical Devices: Portable medical devices that require wireless connectivity could potentially use this module to transmit patient data to central healthcare systems securely and reliably, although specific medical industry standards would need to be adhered to.
- Automotive: In the automotive sector, this module might potentially be used in connected car systems, although strict compliance with automotive industry reliability standards would need to be verified.
Note that these potential industry applications are merely illustrative and must be analyzed and verified by competent engineering and design teams for adherence to specific industry standards and exact application requirements.
About Murata Manufacturing Co Ltd.
Murata Manufacturing Co Ltd. is a global leader in the design and manufacture of electronic components, particularly known for its innovation in the field of ceramic-based passive electronic components and advanced electronic solutions. In the realm of Other Telecom ICs, Murata presents a broad array of products that address a multitude of telecommunication needs spanning from basic connectivity modules to complex communication infrastructure.
For products like LBEE5PL2DL-921 and others in its portfolio, Murata leverages its extensive expertise in material science and electronics to deliver high reliability and performance, catering to diverse telecommunications requirements. The company’s commitment to quality and sustainability is demonstrated through compliance with various environmental standards and proactive participation in eco-friendly initiatives.
Where to Find LBEE5PL2DL-921 by Murata Manufacturing Co Ltd
If you are looking to source the LBEE5PL2DL-921, it is recommended to conduct research on findchips.com. Historically, this part has been available through distributors like Symmetry Electronics, Chip1Stop, Avnet Americas, and Future Electronics. To get the most updated stock levels and competitive pricing, a visit to findchips.com is advisable. Additionally, you can explore alternate parts offered by Murata Manufacturing Co Ltd or other manufacturers by browsing the Other Telecom ICs category on findchips.com.