What Should Buyers Do About the LM324 Demand Surge in 2026?
Buyers sourcing any LM324 variant for Q2 or Q3 2026 production should secure inventory now across multiple authorized distributors. Supplyframe IQ Velocity Insights data shows year-over-year purchase activity up as much as 1,660% for certain variants, and Supplyframe CIQ forecasts indicate pricing will stay elevated through September 2026.
Waiting could result in higher costs. Compare LM324 stock and pricing across authorized distributors now.
Published April 2026 | 6 min read | Sourcing data from Supplyframe IQ Velocity Insights
Next step: Check LM324D availability across distributors.
The LM324 Demand Spike: What the Data Shows
The LM324 family of components is dominating the global sourcing activity index in March 2026. Procurement teams should treat this as a stockpiling or allocation event, not a seasonal blip, and place orders against confirmed Q2 and Q3 demand this week rather than next quarter.
Here are the top variants by purchase surge, year over year:
- LM324QT (STMicroelectronics): +1324D (STMicroelectronics): +791%,660%
- LM324ADR2G (onsemi): +573%
- LM324DR2G (onsemi): +52%
- LM324PT (STMicroelectronics): +35%
Next step: View real-time stock for LM324QT, the highest surge variant.
How Long Will the Demand Spike Last?
Demand will soften gradually through September 2026, but buyers should not wait it out. Supplyframe CIQ amplifier category forecasts show a steady decline, not a sudden correction.
Critical volume requirements for Q2 and Q3 must be locked in now while multiple authorized distributors still carry inventory. Deferring to catch a trough risks being caught short when a single distributor’s inventory depletes.
Next step: Secure LM324ADR2G inventory before further tightening.
How Is the Spike Affecting Pricing?
LM324 pricing will remain elevated through at least Q3 2026. Buyers should compare distributors now to avoid further increases, rather than waiting for a return to pre-surge levels.
Supplyframe IQ CIQ amplifier pricing forecasts show amplifier pricing inflated on a year over year basis through September 2026. The single best cost control lever is comparing live pricing across multiple authorized sources at the same quantity break.
Next step: Compare LM324D pricing across authorized distributors now.
How Is the Spike Affecting Lead Times?
Lead times peaked in Q1 2026 and will ease through Q2. Buyers with flexible schedules should defer non-critical orders to late Q2 or Q3, while buyers with firm Q2 builds should order this week. Amplifier lead times rose 7.9% in Q1 2026 versus Q4 2025, but Q2 2026 lead times are projected to decline 10.7% versus Q2 2025 as inventories recover.
Here’s how this translates into quick decisions:
- If you need immediate supply for Q2 builds: order this week against confirmed demand
- If you need a flexible schedule for Q3 builds: defer to late Q2 when lead times ease
- If your design is dependent on an LM324 variant through Q3: carry safety stock
Next step: Check real time lead times for LM324DR2G.
LM324 Variants: When to Use Each
These are the most commonly sourced LM324 variants. Buyers should prioritize widely available SOIC 14 packages where possible, since TSSOP 14 variants are running tighter.
| Part | Manufacturer | Package | When to Use | Check Availability |
| LM324D | STMicroelectronics | SOIC 14 | Most common, best availability, default choice for new buys | Check LM324D availability across distributors |
| LM324QT | STMicroelectronics | TSSOP 14 | Smaller footprint, currently the tightest supply of the group | Check LM324QT availability across distributors |
| LM324ADR2G | onsemi | SOIC 14 | Interchangeable SOIC 14, alt sourcing when ST is gapped | Check LM324ADR2G availability across distributors |
| LM324DR2G | onsemi | SOIC 14 | Good availability, lower surge than ST variants | Check LM324DR2G availability across distributors |
Next step: Compare all LM324 authorized sources in one view.
Authorized Drop In Alternatives When LM324 Is Unavailable
If your preferred LM324 variant is gapped, the strongest alternative right now is the LM2902 in SOIC 14. It is pin compatible with the LM324 and carries a wider operating temperature range.
Buyers who can tolerate a JFET input should evaluate the TL074 next, and buyers who need tighter offset should use the LM324A.
| Alternate | Key Difference | When to Use | Check Availability |
| LM2902 | Pin compatible, wider temperature range, tighter offset | First fallback when LM324 is gapped | Check LM2902 availability now |
| TL074 | JFET input, lower noise, pin compatible in most LM324 circuits | When low noise matters and JFET input is acceptable. Not drop in replacement. | Check TL074 availability now |
| LM324A | Tightened offset voltage spec, drop in for precision variants | When offset voltage is the gating spec | Check LM324A availability now |
Next step: Compare LM2902 pricing before committing to a redesign.
Where to Buy LM324 from Authorized Distributors
Buyers should purchase only from authorized channels to avoid counterfeit risk, which rises during shortage events.
Findchips aggregates real time stock and pricing from authorized global distributors including Digi Key, Mouser, Arrow, Avnet, and TTI.
Search by variant:
- Check LM324D availability across distributors — STMicroelectronics, SOIC 14
- Check LM324QT availability across distributors — STMicroelectronics, TSSOP 14
- Check LM324ADR2G availability across distributors — onsemi, SOIC 14
- Check LM324DR2G availability across distributors — onsemi, SOIC 14
- Check LM324DR availability across distributors — Texas Instruments, SOIC 14
- Check LM324PT availability across distributors — STMicroelectronics, TSSOP 14
Gray market LM324 inventory carries significant risk of counterfeit or out of spec parts during shortage events. Authorized only.
Next step: Compare all authorized LM324 sources now.
Frequently Asked Questions
| Question | Answer |
| Is the LM324 still safe to design into new products in 2026? | Yes, for cost sensitive and legacy compatible designs. The LM324 family is active across ST, onsemi, and TI, with no EOL signals. Buyers should pair new designs with a qualified LM2902 alternate to de risk supply. Check LM324 authorized sources. |
| What is the most available LM324 alternate right now? | The LM2902 in SOIC 14 is the most available direct substitute with consistent multi-distributor stock. Check LM2902 availability now. |
| How long will the LM324 shortage last? | Demand softens gradually through September 2026. Buyers with Q2 and Q3 needs should act now. Secure LM324ADR2G inventory. |
| Will LM324 lead times improve? | Yes. Q2 2026 amplifier lead times are projected to decline 10.7% versus Q2 2025 as inventories recover. Lead times peaked in Q1 2026. Check LM324DR2G lead times now. |
| Will LM324 pricing come down soon? | Not immediately. Amplifier pricing is forecasted to stay elevated year over year through September 2026. Compare LM324D pricing across distributors. |
| Can LM324 operate on a 5V single supply? | Yes. At 5V the output swings from approximately 0V to 3.5V and the input common mode range extends from 0V to approximately 3.5V. It is widely used in 5V microcontroller systems. Check LM324D stock. |
| Where can I verify LM324 is authentic and not counterfeit? | Purchase only from authorized distributors. Findchips only surfaces authorized distributor inventory. Check authorized LM324 sources now. |
Next step: Check real-time LM324 authorized stock across all variants.