Overview of MBB02070C2151FCT00 by Vishay Intertechnologies
The fixed resistor MBB02070C2151FCT00 by Vishay Intertechnologies is a Metal Film Resistor designed for through-hole mounting. This resistor has a power rating of 0.4W and a resistance value of 2150 ohms, with a tolerance of ±1%. It can handle a maximum voltage of 350V and has a temperature coefficient of 50 ppm/°C, making it highly precise in various temperature conditions. The component is contained within an axial leaded package, which assists in its installation on circuit boards with pre-drilled holes. Factory lead time data at the current writing is 10 weeks. This resistor is packaged in ammo pack format, which facilitates efficient handling and assembly in mass production settings.
Industry Applications for MBB02070C2151FCT00
The following are conceptual industry applications for the MBB02070C2151FCT00 resistor, and their suitability depends on further analysis by engineering and design teams:
- Consumer Electronics: This resistor could be used in devices like TVs and audio equipment where precise voltage regulation and stability over temperature variations are critical. Its high voltage and power handling capabilities, along with a precise tolerance and temperature coefficient, make it suitable for these applications.
- Computing and Data Storage: In computing hardware, such as servers or hard drives, stability and precision are crucial for reliable performance. The MBB02070C2151FCT00’s tight tolerance and stable performance across a wide temperature range could be advantageous in these settings.
- Healthcare: In medical devices, particularly those involving sensitive measurements like electronic stethoscopes or ECG monitors, the precision and reliability of electronic components are imperative. The low tolerance and high temperature coefficient of this resistor might make it useful in such equipment.
- Transportation and Logistics: For electronic systems used in transportation like GPS devices and electronic logging devices (ELDs), consistent performance despite environmental changes is necessary. The robust thermal and voltage ratings of this resistor potentially support such requirements.
Note: These potential industry applications are only illustrative and require verification for adherence to industry standards and specific applications by professional teams.
About Vishay Intertechnologies
Vishay Intertechnologies is a key player in the manufacturing of discrete semiconductors and passive electronic components. Among their offerings, Vishay’s Metal Film Resistors, including the MBB02070C2151FCT00, are recognized for their reliability and precision. These resistors are crafted with metal film technology which provides better performance in terms of accuracy and stability than other resistor types like carbon film. Vishay’s commitment to quality is shown through their compliance with industry standards such as AEC-Q200, which signifies that their components meet stringent automotive sector reliability standards.
Where to Find MBB02070C2151FCT00 by Vishay Intertechnologies
To purchase the MBB02070C2151FCT00, you can explore major distributors such as Avnet Abacus, Future Electronics, Mouser Electronics, and Avnet Americas. However, for current stock levels and pricing, it is recommended to check on findchips.com. On this site, you can also find alternative Metal Film Resistors offered by Vishay Intertechnologies or other manufacturers.