MMBT5551-7-F by Diodes Incorporated

Overview of MMBT5551-7-F by Diodes Incorporated

The MMBT5551-7-F by Diodes Incorporated is a small signal bipolar transistor designed for high-voltage applications. This component features a maximum collector-emitter voltage of 160V and a continuous collector current of 0.6A. It is constructed with a single NPN transistor element and is made from silicon, encapsulated in a plastic, lead-free, small outline package (SOT-23) with three pins. Its key attributes include a DC current gain (minimum hFE) of 30 and a transition frequency of 100 MHz, making it suitable for switching applications. The MMBT5551-7-F is compliant with RoHS, REACH, and is characterized by a moisture sensitivity level of 1, indicating its resilience in humidity-sensitive environments. With an operating temperature range from -55 °C to 150 °C, this component is adaptable to various challenging operational climates.

Industry Applications for MMBT5551-7-F

The MMBT5551-7-F could potentially be utilized across several industrial domains. However, it is important to note that these applications are hypothetical and should be validated by engineering teams specific to each industry to ensure compliance with relevant standards and requirements. Here are some possible applications based on the characteristics of the MMBT5551-7-F:

  • Consumer Electronics: Devices such as power management systems in consumer electronics could potentially employ this transistor due to its high voltage tolerance and switching capabilities. For example, it might be used in the voltage regulation modules of personal computers or televisions.
  • Industrial Automation: In industrial automation, controlling large loads often requires components capable of handling high voltages and currents. The MMBT5551-7-F, with its specifications, could possibly be used in the manufacturing of motor controllers or automation equipment.
  • Audio and Video Systems: Audio amplifiers and other audio processing equipment that require discrete components for signal modulation could potentially use this transistor. Its high transition frequency makes it suitable for audio frequency applications.
  • Electronic Manufacturing: For electronic manufacturing, especially in the development of prototypes and small scale production, this transistor could be utilized for designing and testing circuit boards that require high-voltage bipolar transistors.

Please remember that these suggested uses are illustrative and require further analysis and verification by specialized personnel.

About Diodes Incorporated

Diodes Incorporated is a leading manufacturer in the semiconductor market, known for its wide range of transistors including those within the category Small Signal Bipolar Transistors. In addition to the MMBT5551-7-F, Diodes Incorporated produces a variety of similar components which cater to diverse electronic applications. Their products are distinguished by their reliability, innovation, and compliance with international environmental standards such as RoHS and REACH. The company’s dedication to quality and sustainability makes it a trusted name in the component manufacturing industry, supporting customers in achieving both technically effective and environmentally responsible outcomes.

Where to Find MMBT5551-7-F by Diodes Incorporated

To purchase the MMBT5551-7-F, one should consider using platforms such as findchips.com. On findchips.com, you can compare current availability and pricing from various distributors. Typically, this part has been available from distributors such as LCSC, Mouser Electronics, DigiKey, and Newark, among others. However, for the most up-to-date information on stock levels and competitive pricing, checking through findchips.com is advisable. Additionally, if you’re considering alternatives, the Small Signal Bipolar Transistors link on findchips can be used to explore other similar parts that might be offered by Diodes Incorporated or other manufacturers.

Compare pricing for MMBT5551-7-F and other Small Signal Bipolar Transistors at findchips.com