Overview of MPC564CZP66 by NXP Semiconductors
The MPC564CZP66 is a 32-bit RISC microcontroller featuring 512KB of flash memory, designed and manufactured by NXP Semiconductors. This part is encapsulated in a 388-pin PBGA (Plastic Ball Grid Array) package, adhering to a 27 x 27 mm footprint with a 1 mm pitch. Although not recommended for new designs as indicated by its lifecycle status from findchips.com, MPC564CZP66 remains a viable option for ongoing or legacy projects. Notably, it operates within the industrial temperature range of -40 °C to +85 °C and requires a nominal supply voltage of 2.6V, with an acceptable range from 2.6V to 2.7V.
Despite not being ROHS compliant and its qualification status as “not qualified,” this microcontroller supports applications that can accommodate these restrictions. Some key characteristics include a maximum clock frequency of 66 MHz, a 24-bit address bus width, 32 external data bus width, and 32KB of RAM. Its technological foundation is CMOS, and it supports surface mounting for assembly.
Industry Applications for MPC564CZP66
The potential industry applications of the MPC564CZP66 span various sectors, thanks to its specialized feature set. While tagged for automotive applications, there are other realms where this microcontroller could significantly contribute. Given the possible implementations of this device, it’s critical to remember these scenarios are illustrative and should be thoroughly vetted by an engineering team.
- Automotive: Given its specified application, the MPC564CZP66 could serve in engine control modules, transmission controllers, and other embedded systems within vehicles. The rigorous operating temperature range suits the harsh automotive environment.
- Industrial Control: With its robust temperature range and input/output capabilities, it could find applications in industrial automation and control systems, such as process controllers, robotic arms, or sensor nodes where precision and reliability are crucial.
- Consumer Electronics: Potential use in high-end consumer electronics that require complex user inputs and real-time processing, including gaming consoles, advanced personal digital assistants, and Smart Home devices.
- Communications Equipment: Its data handling capabilities may be applied to communication infrastructure equipment such as routers, switches, or base station controllers where processing throughput and reliability are mandatory.
Note: These applications are conceptual and require confirmation for suitability by design and engineering teams.
About NXP Semiconductors
NXP Semiconductors is a global leader in the development and manufacturing of semiconductor solutions, particularly in the Microcontrollers and Processors arena. With a rich history that spans several decades, NXP is recognized for its contribution to advancements in automotive, industrial, and consumer electronics through innovative semiconductor technologies. The MPC564CZP66, alongside its comprehensive portfolio of microcontrollers, showcases NXP’s commitment to providing robust and versatile computing solutions. NXP’s offerings are characterized by their reliability, performance, and adherence to the latest industry standards, making them a preferred choice for engineers and designers worldwide.
Where to Find MPC564CZP66 by NXP Semiconductors
Finding the MPC564CZP66 for purchase can be a key step in the procurement process, and utilizing resources like findchips.com can greatly simplify this task. By visiting findchips.com, you can identify current stock levels, get pricing from various distributors, and compare options efficiently. Historically, the MPC564CZP66 has been available from distributors such as EBV Elektronik, Avnet Silica, Mouser Electronics, Avnet Americas, DigiKey, and Newark. However, for the most current availability and competitive pricing, it’s best to rely on findchips.com. Additionally, for those seeking alternative solutions or comparable parts offered by NXP Semiconductors or other manufacturers, exploring the Microcontrollers category on findchips.com is advisable.