Overview of MT29F128G08AKCABH2-10ITZ:A by Micron Technology Inc.
The MT29F128G08AKCABH2-10ITZ:A by Micron Technology Inc. is an obsolete 128 gigabit Flash memory IC housed in a 100-terminal plastic epoxy ball grid array (BGA) package. It uses CMOS technology and is designed for parallel interface. Features include a maximum access time of 20 nanoseconds, industrial temperature grade ranging from -40°C to 85°C, and a command user interface. This component provides an array structure of 16Gx8, which means it organizes data in blocks with 16 billion cells that are 8 bits wide.
As a Flash memory component, listed under the subcategory of Flash Memories within the Memory category, this part has a significant storage capacity and is geared towards applications requiring storage solutions where data integrity and speed are critical. Even though this part is marked as obsolete, its capabilities still offer considerable relevance in legacy systems or specific applications where newer versions or replacements are not viable due to various constraints such as system architecture or compatibility requirements.
Industry Applications for MT29F128G08AKCABH2-10ITZ:A
The application areas for Flash memories like MT29F128G08AKCABH2-10ITZ:A are vast, given their importance in storing large volumes of data and enabling quick access. Here, let’s discuss how such Flash memory solutions could potentially be used in various industry applications:
- Computing and Data Storage: Given its high density and command interface, this Flash memory could potentially serve in data centers for server storage, handling tasks that require rapid access to stored data without significant latency.
- Consumer Electronics: Devices such as digital cameras, gaming consoles, and high-end audio equipment might use high-capacity Flash memories for data buffering and rapid access to media files.
- Industrial Automation: Systems that monitor and control industrial equipment with stringent data logging requirements could utilize such high-capacity, durable memories due to its operating temperature range and robustness in harsh environments.
- Electronic Manufacturing: Used in sophisticated manufacturing systems for storing firmware updates, configuration logs, and operational data to enhance precision and efficiency in product assembly lines.
Note that these potential industry applications of MT29F128G08AKCABH2-10ITZ:A are conceptual/illustrative. Analysis and verification by engineering and design teams are necessary to ensure adherence to industry standards and specific application requirements.
About Micron Technology Inc.
Micron Technology Inc. is a global leader in memory and storage solutions, renowned for its wide array of memory technologies including DRAM, NAND, NOR Flash, and 3D XPoint memory. For Flash Memories, Micron offers products like the MT29F128G08AKCABH2-10ITZ:A which serve as essential components in a variety of electronic devices. The company provides memory solutions that are used in everything from computing, networking, and server applications, to mobile, embedded, consumer, automotive, and industrial applications.
Micron has been pivotal in progressing flash memory technology, and despite the obsolescence of certain models such as the MT29F128G08AKCABH2-10ITZ:A, it continually innovates to meet modern data storage requirements. Micron’s ongoing research and development efforts ensure they stay at the forefront of technology, offering both high performance and reliability in their memory solutions.
Where to Find MT29F128G08AKCABH2-10ITZ:A by Micron Technology Inc
To locate and purchase the MT29F128G08AKCABH2-10ITZ:A, visiting findchips.com is advisable where one can find detailed stock levels and pricing from various distributors. Although historically available at distributors like DigiKey, current stock and availability can vary. The link to Flash Memories at findchips can also be used to compare and possibly alternate parts offered by Micron Technology Inc or other manufacturers.