MTA8ATF1G64HZ-3G2R1 by Micron Technology Inc

Overview of MTA8ATF1G64HZ-3G2R1 by Micron Technology Inc.

The MTA8ATF1G64HZ-3G2R1 by Micron Technology Inc. is a DDR4 SDRAM module that features 8GB of memory capacity in a 260-pin small outline dual in-line memory module (SO-DIMM) format. Designed for use in systems that require high-speed, large-capacity memory, such as advanced computing devices, this DDR4 module offers enhancements in speed and power efficiency over its predecessors like DDR3. DDR4 technology provides higher module density and lower voltage requirements, alongside faster data transfer rates.

Micron, as the manufacturer of this memory module, is a leader in the global semiconductor industry, particularly known for its innovations in memory and storage solutions. The MTA8ATF1G64HZ-3G2R1 meets industry standards for quality and reliability, complying with RoHS (Restriction of Hazardous Substances) which ensures that it is free from specific hazardous materials found in electrical and electronic products. Though the REACH (Registration, Evaluation, Authorization, and Restriction of Chemicals) compliance status is unknown, the part remains active in production and has a general factory lead time of approximately 13 weeks and 3 days at the time this data was compiled.

Industry Applications for MTA8ATF1G64HZ-3G2R1

The MTA8ATF1G64HZ-3G2R1 module, belonging to the DRAMs subcategory, could potentially serve various industry applications where large capacity and data rate speeds are crucial. Different industries might find this memory module suitable, depending on their specific technology requirements.

  • Consumer Electronics: This memory module could potentially be used in high-performance consumer electronics such as gaming consoles, high-end laptops, and advanced photography and video equipment. The fast data transfer rates and large memory capacity are essential for devices that require quick loading times and efficient multitasking capabilities.
  • Computing and Data Storage: In the computing sector, the MTA8ATF1G64HZ-3G2R1 might be found in data centers and server farms, which require robust, efficient, and scalable memory solutions. Its capabilities would be suited to support complex computations and large-scale data processing tasks essential for cloud computing and big data analytics.
  • Education and Research: Academic institutions and research facilities could utilize this DRAM module in workstations and computing clusters that are used for scientific simulations, data analysis, and computational research projects. The enhanced speed and capacity ensure that these applications run efficiently.

Nevertheless, these potential applications are conceptual and would require thorough analysis and verification by engineering and design teams to ensure they comply with the specific standards and requirements of the industries mentioned.

About Micron Technology Inc.

Micron Technology Inc. is a major player in the field of semiconductor engineering, primarily known for its significant contributions to the DRAMs and broader memory market. The company is involved in the development of many memory technologies that include DRAM, NAND, and NOR flash memory. Among these, its innovations in DRAM technology, including examples like MTA8ATF1G64HZ-3G2R1, have positioned it as a key supplier for many electronics and data-related services. Micron continuously invests in next-generation technologies to address the ever-growing demand for higher memory capabilities in various sectors, from consumer electronics to industrial applications.

Where to Find MTA8ATF1G64HZ-3G2R1 by Micron Technology Inc

For sourcing the MTA8ATF1G64HZ-3G2R1, potential buyers should consider conducting thorough research on findchips.com. The website provides information on current stock levels, pricing, and available distributors. Although historically the part has been available at distributors such as LCSC, Avnet Americas, Mouser Electronics, Avnet Silica, DigiKey, and Farnell, stock levels and availability may vary. To explore alternate parts as well as other offerings from Micron Technology Inc. or competitive manufacturers, accessing the DRAMs section might provide additional beneficial options.

Compare pricing for MTA8ATF1G64HZ-3G2R1 and other DRAMs / Memory at findchips.com