MX25U25645GZ4I00 by Macronix International Co Ltd

Overview of MX25U25645GZ4I00 by Macronix International Co Ltd.

The MX25U25645GZ4I00 is a high-performance flash memory device featuring 256 Mbit storage capacity, with an operational temperature range of -40 to 85 degrees Celsius. This device comes in an 8WSON (Very Very Thin Small Outline No Leads) package and utilizes Serial Peripheral Interface (SPI) and Quad SPI communication protocols for data transfer. Macronix International Co Ltd., the manufacturer of this component, has designed it to be operational under a wide range of environmental conditions, making it suitable for diverse applications.

This component is recognized for its robustness, evidenced by its industrial temperature grade and synchronization capability that supports a maximum clock frequency of 166 MHz. This Flash memory part has important features like a serial interface and programming voltage requirement of 1.8 V. It conforms to environmental and safety standards such as RoHS and its package design reflects a dedication to minimalistic and efficient use of space with significant considerations toward heat dissipation. Its memory organization allows for a versatile configuration supporting various data widths that enhance its adaptability in different system architectures. At the time of this writing, the typical factory lead time for this part is 10 weeks.

Industry Applications for MX25U25645GZ4I00

The following are potential industry applications for the MX25U25645GZ4I00, conceptualized based on its high operational reliability, wide temperature range, and robust memory capacity. These illustrative uses should be further evaluated by engineering and design teams for adherence to specific application requirements and industry standards:

  • Industrial Automation: The MX25U25645GZ4I00 could potentially be integrated into programmable logic controllers (PLCs) or other automation hardware needing dependable flash memory for configuration or logging tasks which operate within a wide range of temperatures.
  • Consumer Electronics: Devices such as digital cameras and portable music players, which require high-density, reliable memory storage, might find this flash memory useful for managing large volumes of data with fast access times.
  • Telecommunications: Given its robust operational parameters, this memory device might also be suitably integrated into telecommunications equipment, such as networking hardware that requires long-term data integrity and fast data access.
  • Computing and Data Storage: In cloud storage and other large-scale data centers, reliable memory parts such as the MX25U25645GZ4I00 could be used in systems that manage critical data requiring quick retrieval and resistance against environmental factors.

It is imperative to understand that these are promising applications theoretically evaluated; exact fit and alignment to applications must be verified through detailed technical assessment.

About Macronix International Co Ltd.

Macronix International Co Ltd. is an established leader in the development and manufacturing of non-volatile memory, particularly in the Flash Memories segment. The firm is well-known for its commitment to providing advanced memory solutions that meet rigorous industry performance and reliability standards. The MX25U25645GZ4I00 is an example of Macronix’s innovation in flash memory that emphasizes durability, high memory density, and efficient data handling.

The company supports a wide array of memory technologies and has consistently shown a dedication to advancing flash memory technology. Their products, such as MX25U25645GZ4I00, are integral in numerous devices across various sectors owing to their quality and reliability.

Where to Find MX25U25645GZ4I00 by Macronix International Co Ltd

To purchase MX25U25645GZ4I00 or to find alternate parts that might be offered by Macronix International Co Ltd or other manufacturers, visit the Flash Memories subcategory on findchips.com. Distributors where this part has historically been available include Avnet Americas, Future Electronics, DigiKey, and Farnell. However, current stock levels and pricing should be checked on FindChips to ensure the most accurate and up-to-date information.

Compare pricing for MX25U25645GZ4I00 and other Flash Memories / Memory at findchips.com