Overview of P822601 by Kyocera AVX Components
The P822601 is an embedded antenna designed for the RF/microwave frequency range, specifically covering frequencies from 1.7 to 2.7 GHz with a gain of 3.4dBi. This component is part of the RF/Microwave Antennas subcategory, emphasizing its role in RF and microwave applications. Manufactured by Kyocera AVX Components, it boasts a linear polarization and is capable of operating not only within its nominal frequency range but also at extended bands from 1710 to 2200 MHz and 2500 to 2700 MHz, adding versatility to its use in a wide array of RF applications.
With a characteristic impedance of 50 Ω and designed for surface mounting, the P822601 is equipped with seven terminals and is noted for its non-omnidirectional pattern, which allows for targeted signal transmission and reception. Suitable for transmitting up to 2W of power and featuring a maximum Voltage Standing Wave Ratio (VSWR) of 2.5, it aligns with both RoHS and REACH compliance codes, ensuring its suitability for global markets. The antenna is currently in an active part life cycle phase, with a factory lead time of 10 weeks and 3 days as of the current writing.
Industry Applications for P822601
The P822601 embedded antenna is tailored for a broad range of industry applications, tapping into the functionalities required by modern wireless systems. While this antenna has a strong affinity for advanced communications technology, several sectors stand out as particularly relevant for its incorporation:
- Space Technology and Aerospace: Given its high frequency and targeted transmission capabilities, the P822601 could potentially serve as a component in satellite communication systems or within aviation communication technology. It’s crucial, however, for engineering and design teams to verify its applicability based on specific environmental and functional requirements.
- Transportation and Logistics: This antenna might be integrated into systems for real-time fleet tracking, cargo monitoring, or as part of the infrastructure for advanced logistics operations, providing reliable communication capabilities essential for this sector’s operations.
- Renewable Energy: In the context of renewable energy sources, the P822601 could aid in the wireless monitoring and management of remote installations, such as wind turbines or solar panels, facilitating efficient operation and maintenance through enhanced connectivity.
- Robotics and Drones: For drones and robotic systems that require robust communication links for control, navigation, or data transmission, the specific attributes of the P822601 make it a contender for integration into these technologies.
These potential applications are only illustrative and require thorough analysis and verification by engineering and design teams to ensure compatibility and performance within the specified environments and systems.
About Kyocera AVX Components
Kyocera AVX, a leader in the manufacturing of advanced electronic components, has developed a reputation for its innovative approach to RF/microwave technology. Within the realm of RF and Microwave, Kyocera AVX has been instrumental in pushing the boundaries of what’s possible with components such as the P822601 antenna and other similar devices. These components are known for their quality, reliability, and cutting-edge technology, fitting seamlessly into a wide array of applications—from consumer electronics to industrial systems. The company’s focus on research and development has led to products that not only meet current demands but also anticipate future needs in the rapidly evolving RF/microwave landscape.
Where to Find P822601 by Kyocera AVX Components
To purchase the P822601 or explore alternative RF/Microwave Antennas, findchips.com serves as an essential resource for procurement specialists and engineers alike. The platform offers current stock levels, pricing, and detailed specifications for components by Kyocera AVX and other leading manufacturers.
In the past, the P822601 has been available at distributors such as Symmetry Electronics, TME, Future Electronics, and DigiKey. Since availability can vary, it is recommended that interested parties consult findchips.com to get updated information on distributors, stock status, and competitive pricing for this part and other RF/microwave antenna solutions.