PESD5V0L2BT,215 by Nexperia

Overview of PESD5V0L2BT,215 by Nexperia

The PESD5V0L2BT,215 is a low capacitance double bidirectional ESD protection diode packaged in a SOT-23 form factor (TO-236). This device is designed for effective electrostatic discharge (ESD) protection, accommodating an operating voltage of 5V with a maximum clamping voltage of 28V. The configuration is common cathode, utilizing two diode elements made from silicon, which helps manage transient voltage spikes that might occur in electronic circuits.

With a power dissipation capacity of up to 350W, this diode is well-suited for various applications needing robust protection from ESD events. The PESD5V0L2BT,215 is compliant with the RoHS directive, aligning with industry standards aimed at reducing hazardous substances in electronic products. This diode is part of the PESD series and has been in the market since its introduction on February 17, 2017. As of the current writing, the part is noted to have a factory lead time of approximately 8 weeks, which is relevant for procurement and planning purposes.

Industry Applications for PESD5V0L2BT,215

The PESD5V0L2BT,215 could potentially find applications across various industries, supporting the design of sensitive electronics that must withstand ESD events. Below are some examples of possible use cases:

  • Consumer Electronics: This part might be incorporated in smartphones or tablets where ESD protection is critical to maintain device integrity and longevity. Attributes such as the low capacitance and fast response time could help preserve signal integrity in high-speed data lines.
  • Telecommunications: In network equipment, such as routers or modems, the PESD5V0L2BT,215 might be used to safeguard against voltage spikes that could occur due to ESD events. The device’s dual bidirectional configuration could provide comprehensive protection in these applications.
  • Automotive Electronics: Potentially useful in automotive electronics, particularly in non-critical applications that do not require stringent automotive standards, the PESD5V0L2BT,215 could offer ESD protection for infotainment systems or sensor modules. However, special attention must be given to compliance with AEC-Q100 or AEC-Q101 standards for safety and reliability.
  • Industrial Automation: In robotics or industrial control systems, this diode might help protect sensitive control circuits from transient voltages caused by ESD. The operating temperature range of -65 °C to 150 °C enhances its adaptability in varied industrial environments.
  • Medical Imaging: In diagnostic imaging equipment, the PESD5V0L2BT,215 might be incorporated to ensure the reliability and performance of sensitive electronic components. As with automotive and healthcare applications, specific standards must be adhered to for medical use cases.

It is important to note that these potential industry applications are conceptual and illustrative; they require thorough analysis and verification by engineering and design teams to ensure compliance with industry standards and specific application requirements.

About Nexperia

Nexperia is a global semiconductor company that specializes in discrete, logic, and MOSFET devices. They have a broad portfolio of products, including ESD protection components such as the PESD5V0L2BT,215, which is part of their comprehensive range of transient suppressors in the diode category. Nexperia focuses on providing reliable and efficient solutions for various applications, ensuring their components meet the necessary performance standards prevalent in today’s electronic systems. Similar parts in their range could include other ESD protection diodes that cater to different voltage and configuration requirements. Their strong commitment to quality and innovation makes them a noteworthy manufacturer in the electronic components industry.

Research Price and Stock for PESD5V0L2BT,215 by Nexperia on Findchips.com

For those interested in acquiring the PESD5V0L2BT,215, it is recommended to research stock and pricing through Findchips.com. This platform can provide valuable insights not only into the availability but also into alternative parts in the Transient Suppressors category, which may be offered by Nexperia or other manufacturers. Historical distribution sources for this part include:

  • New Advantage Corporation
  • EBV Elektronik
  • Chip One Stop
  • Avnet Silica
  • DigiKey

However, it is important to check Findchips for the most current stock levels and pricing, as availability can vary frequently based on demand and supply conditions.

Compare pricing for PESD5V0L2BT,215 and other Transient Suppressors / Diodes at findchips.com