From Prototype to Production: The Sourcing Review Your Dev-Board Parts Never Got

Moving a design from prototype to production usually means rechecking parameters like power, thermal and EMC. However, this transition rarely entails rechecking the parts themselves. 

That omission could have consequences as designs transition to the production phase. One major repercussion could arise from the use of dev-board favorites like the AMS1117 and STM32F103C8T6, which can create uncertainty as these are names shared by many chips from many suppliers, although the actual parts may have varying specifications.

A short sourcing review at the engineering validation test (EVT) handoff phase can resolve this uncertainty by transforming those names into locked part numbers.

How Do Prototype Parts End Up in Production?

Most prototypes are built from what is close at hand. An engineer copies the power section from a dev board schematic, drops in the module used by the reference design and orders whatever header matches the cables already on the bench. Every one of those choices is reasonable. 

However, the trouble starts when the prototype works. Each review after that point asks whether the design performs, not whether its parts can be sourced reliably for the life of the product. The schematic gets refined, the layout gets tightened and the BOM keeps the same lines it had on day one.

By the time procurement sees the BOM, a part chosen for convenience has become a part that the product depends on. Nobody decided to put a convenience part into production. It simply never got a second look.

That makes this a handoff problem, not a discipline problem. Our earlier piece on sourcing as a design constraint made the general case for bringing availability considerations into design reviews. The prototype handoff is the single point where that check does the most good for the least effort.

Next step: Check availability for the parts on your current prototype BOM with a Findchips search.

Why Is a Familiar Part Name Not a Part Number?

Some parts are so common that engineers order them by name. The AMS1117 is the clearest example. It started as a regulator from Advanced Monolithic Systems, and the name became so widely used on 3.3 V microcontroller boards that it now works more like a category than a product.

Many manufacturers sell a part called AMS1117 or something close to it. Established suppliers such as onsemi, STMicroelectronics and Texas Instruments sell their own 1117-series regulators too. These parts share a footprint and a nominal output voltage. They do not always share the rest of the datasheet.

Dropout voltage, quiescent current, output capacitor requirements and protection features can differ from one maker to the next. The original AMS1117 datasheet calls for a tantalum output capacitor for stability, which matters if the production board uses ceramics. Independent testing of low-cost parts sold under the name AMS1117 has revealed units without working over-temperature shutdown, a feature that legitimate datasheets list.

The same pattern shows up in microcontrollers. Low-cost boards based on the STM32F103C8T6 microcontroller often carry compatible chips from other makers, and some of those chips are marked as something they are not. A compatible MCU can be a fine design choice when it is chosen on purpose. It becomes a risk when nobody knows it is there.

The lesson for production is simple. A name on a schematic tells you what a part is supposed to do. Only a manufacturer part number tells you what you are actually buying.

Next step: Compare AMS1117 and 1117-series regulators across manufacturers on Findchips.

Which Dev-Board Parts Carry the Most Production Risk?

The parts that cause trouble at the handoff stage tend to be the ones that made prototyping easy. The table below covers the most common examples and what to pin down before each one ships in volume.

PartWhy It Shows Up on PrototypesProduction Sourcing RiskWhat to Lock Down
AMS1117-3.3Default regulator on many 3.3 V dev boardsMany makers under one name; specs and protection varyManufacturer MPN, output capacitor requirement, qualified alternates
STM32F103C8T6Familiar from low-cost boards and tutorialsCompatible and remarked chips circulate in low-cost channelsAuthorized sourcing and a deliberate decision on any compatible MCU
ESP32-S3-WROOM-1-N16R8Common dev kit configuration with large flash and PSRAMFirmware depends on the memory variant; octal PSRAM variants reserve several GPIO pinsExact module variant plus a fallback variant tested with the firmware
AO3400A and AO3401ACheap logic-level SOT-23 MOSFETs on many hobby boardsWidely copied; parts sold under these numbers vary in specsManufacturer, key datasheet specs and approved alternates
JST PH and XH headersMatch the cables already on the benchHeader, housing and crimp are separate MPNs; look-alike housings may not mate reliablyFull mating set from one series, sourced together
NE555Familiar, forgiving timerBipolar and CMOS versions behave differently on supply range and currentBipolar or CMOS decision and a manufacturer MPN

None of these parts is a bad choice. Each one is a reasonable production part when the exact device, maker and channel are known. 

Connectors deserve special attention because the risk is split across several part numbers. Our guide to JST connector types covers how to source the full mating set, and our small-signal MOSFET cross-reference explains what has to match before swapping parts like the AO3400A.

Next step: Search any part from your prototype BOM on Findchips to see which manufacturers and authorized distributors carry it.

What Does Current Design Activity Show?

Supplyframe IQ data suggests current design activity is not a niche concern. In September 2026, design-side activity rebounded broadly, and the most active parts read like a prototyping kit. ESP32-S3 modules, the STM32F103C8T6, the AMS1117-3.3, the AO3400A and AO3401A, NE555 variants and 11 JST wire-to-board connectors all ranked among the top-100 design-side part numbers.

That list reflects what engineers are designing with right now. Some of those designs will stay on the bench. Others will move into production with the parts they started with, which is exactly when the sourcing review should happen.

Next step: See which parts engineers are searching most on Findchips.

How Do You Run a Sourcing Review at the EVT Handoff?

This type of review does not need to be a new process. It is one pass through the BOM with a different question: Can we buy exactly this part from a trusted channel for the life of the product? Six checks cover most of it: 

  1. Flag inherited lines. Mark every part copied from a dev board, reference design or earlier project. These are the lines nobody chose on purpose.
  2. Resolve names to manufacturer part numbers. Replace generic names and loose descriptions with a full MPN from a named manufacturer, including package and temperature grade.
  3. Qualify alternates by datasheet, not by name. Two parts with the same name are not automatically interchangeable. Compare the specs your circuit depends on, then list approved alternates by MPN.
  4. Check lifecycle and source count. Confirm each part is active and carried by more than one authorized distributor. A single source is fine when it is a known decision.
  5. Lock module and variant choices. For modules and parts with memory or feature variants, record the exact variant the firmware was tested on and qualify a fallback.
  6. Name approved channels. Record approved manufacturers on the approved vendor list so a buyer under schedule pressure does not reach for a look-alike.

When done at the EVT handoff, this process takes hours. When conducted after a production build fails incoming inspection, it can take weeks and a board respin.

Next step: Check lifecycle status and distributor coverage for every line on your BOM with Findchips.