PTN3222CUKZ by NXP Semiconductors

Overview of PTN3222CUKZ by NXP Semiconductors

The PTN3222CUKZ is an interface circuit designed to function as a redriver for signals transitioning from EUSB2 to USB2. Packaged in a WLCSP-12 format, it represents a specialized solution developed by NXP Semiconductors to enhance signal integrity in USB data transfer applications. The element of redriving is critical in applications where signal degradation may occur due to long-distance transmissions or where the quality of the transmission medium might introduce losses.

According to its specifications, this part has a Moisture Sensitivity Level (MSL) of 1, indicating that it can handle exposure to moisture at a high level without risk of damage, which is crucial for reliability and longevity in various application environments. It can withstand a peak reflow temperature of 260°C, although the maximum duration at this temperature isn’t specified. This insight into thermal resilience is crucial when considering fabrication processes involving high-temperature phases. As of the latest update, the factory lead time for this component is approximately 16 weeks.

Industry Applications for PTN3222CUKZ

The PTN3222CUKZ finds applicability across various high-tech industries due to its functionality as an interface circuit in USB data transfer systems. Below are a few industries where this part could potentially play a critical role:

  • Consumer Electronics: In consumer devices such as laptops, smartphones, and tablets, the PTN3222CUKZ might be used to facilitate enhanced USB interface capabilities, offering more reliable data transfer rates required for high-performance consumer electronics.
  • Computing and Data Storage: For servers and data centers where multiple USB connections are common, this component could potentially help maintain data integrity and speed, enhancing the overall system reliability and user experience.
  • Telecommunications: The telecommunications industry could utilize this part to ensure clearer and more reliable signal transmission between various network devices, especially in situations involving extended cable runs where signal integrity is paramount.
  • Industrial Automation: In the realm of industrial automation, where equipment must communicate seamlessly over various interfaces, the PTN3222CUKZ could be used to ensure reliable USB communications between controllers and peripheral devices.

Please note that these potential industry applications are conceptual and illustrative. The utility and compliance of this component with industry standards and specific application requirements would require thorough investigation and verification by engineering and design teams.

About NXP Semiconductors

NXP Semiconductors is a leading technology company well-known for its broad portfolio of solutions in semiconductors and electronic components. Within the realm of Other Interface ICs, NXP designs and manufactures a diverse array of products, including those like the PTN3222CUKZ. These components play essential roles in managing communication and functionality between various electronic systems, crucial for achieving desired outputs and system efficiencies.

Their products are utilized in numerous technology-driven industries, catering to needs ranging from basic consumer electronics applications to sophisticated industrial and telecommunication systems. The innovative drive and quality assurance practices at NXP Semiconductors ensure that their products consistently meet the high standards required in today’s advanced electronic and technological frameworks.

Where to Find PTN3222CUKZ by NXP Semiconductors

To purchase the PTN3222CUKZ, potential buyers should consider exploring options on platforms like findchips.com. On this site, users can view current stock levels, compare pricing, and check availability from various distributors. Historically, distributors such as Chip1Stop, Avnet Americas, Mouser Electronics, DigiKey, and Farnell have carried this part. However, availability can vary, so checking the most current data on FindChips is recommended.

Additionally, for alternatives within the category of Other Interface ICs, FindChips provides a resource for comparing similar parts from NXP Semiconductors or other manufacturers, ensuring that designers and procurement professionals can find the best match for their application requirements.

Compare pricing for PTN3222CUKZ and other Other Interface ICs / Drivers And Interfaces at findchips.com