Overview of QPA4586ATR13 by Qorvo
The QPA4586ATR13 from Qorvo is a cascading Silicon Germanium (SiGe) heterojunction bipolar transistor (HBT) MMIC amplifier. It operates up to a maximum frequency of 4000 MHz and is housed in a SOT-86 plastic/epoxy package featuring four pins. This wide band low power amplifier comes in tape and reel packaging, making it suitable for high-volume applications. Its characteristic impedance is 50 Ohms, and it features a gain of 18.6 dB with a maximum continuous wave (CW) input power of 18 dBm.
This amplifier was introduced to the market on October 24, 2016, and is designated as RoHS compliant and REACH compliant. Notably, it is also classified under the IHS ‘End Of Life’ lifecycle phase, and its terminal finish is matte tin (Sn). As of the current date, this part has a factory lead time of 16 weeks. Its operational range is quite robust, functioning between -55 °C and 105 °C, which indicates its suitability for varying environmental conditions.
Industry Applications for QPA4586ATR13
The versatile characteristics of the QPA4586ATR13 allow it to be applied in a range of industries. These applications, however, are potential uses and should be further analyzed and verified by engineering teams to meet specific standards and requirements of the intended application. Below are several industries where this part could potentially be applied:
- Telecommunications: It might be used in RF signal chains, potentially fitting into equipment such as cellular base stations where amplification of wide-band signals is required. The operating frequency and gain properties of QPA4586ATR13 might make it suitable for such applications.
- Consumer Electronics: This part could potentially be used in designing RF modules for wireless-enabled consumer devices such as smartphones, tablets, or wireless modems. Its compact SOT-86 package and surface-mount configuration might be beneficial for the miniaturization of these devices.
- Internet of Things (IoT): Due to its low power consumption and wide operating temperature range, QPA4586ATR13 could potentially fit into IoT devices which require reliable operation over variable climatic conditions and extended periods, particularly in remote sensing and communication devices.
Note: These industry applications are purely illustrative and conceptual and should be validated by respective industry professionals per applicable standards and usage requirements.
About Qorvo
Qorvo is a leading provider in the field of RF solutions, particularly excelling in the creation and production of RF/Microwave Amplifiers like the QPA4586ATR13. Their products are known for pushing the boundaries in the RF sector which finds applications across multiple high-tech industries including aerospace, mobile devices, and IoT. In addition to the QPA4586ATR13, Qorvo manufactures a broad range of similar components which leverage advanced materials like GaN (Gallium Nitride) and SiGe (Silicon Germanium), ensuring state-of-the-art performance for RF and microwave applications.
Where to Find QPA4586ATR13 by Qorvo
To source the QPA4586ATR13, using an online electronic component aggregator like findchips.com is advisable. This site can aid in comparing availability and pricing from different distributors. Historically, the part has been available from distributors such as Mouser Electronics, Avnet Americas, and DigiKey. To find current stock levels and potential purchasing options, visit findchips.com. Additionally, should you consider alternatives within the same category, the RF/Microwave Amplifiers link may provide insights into similar parts offered by Qorvo or other manufacturers.