Second sourcing has always been a first line of defense against shortages, demand spikes and other hazards that routinely disrupt product lifecycles. Sometimes a vendor discontinues a part, other times prices go up, and on other occasions, the component experiences a severe supply constraint, accompanied by a soaring lead time.
Recent years have shown that current second sourcing strategies aren’t effective. Not when the issues go past the vendor and straight to the foundry or the other foundational layers of the supply chain. In these scenarios, your second source is just the same bet with a different package. Join us as we explore how second sourcing strategies can find new life in 2026 and beyond.
The Pattern Everyone Will Recognize
Here is a scenario many will recognize: A part family tightens, teams pull out the qualified alternate, and it just so happens that this alternate has an identical lead time of 30 weeks. Sound familiar?
Logic dictates that this is expected, because everyone else rushed to secure the same alternate and crowded the space. To be clear, this does happen, but it doesn’t explain situations where lead times for the alternate started extending before the substitution wave arrived, or where a third or fourth option moved in the same direction at the same time.
It’s easier to say that this happened due to the market chasing an alternative, but the reality is that the qualification was incomplete. It lacked the full context surrounding the part. It side-stepped the greater problem. In essence: if a primary and qualified alternate part move together in terms of lead time and availability, we should consider the possibility that they are coupled to something else.
And if that is indeed the case, then how do we fix it?
Supplier Count is the Wrong Measure
Seeing a number of qualified sources on a BOM is comforting because it says that the teams have alternates in case supply challenges arise. However, this alone is not enough to say the line is protected.
A part with three alternates that are all fabbed on the same process and in the same foundry is more exposed than a part with one alternate that is built in a different region, on a different process.
Counting suppliers measures effort, but it does not gauge independence. It’s also hard to gauge independence based solely on suppliers alone. Naturally, there is objection to this approach, due to the sheer cost of time and effort.
After all, most teams cannot audit their vendor’s manufacturing footprints. Fab assignments are not often disclosed, and they change without notice. Demanding a full dependency map before approving a second source will cause the entire process to grind to a halt.
However, the answer to an unverifiable claim isn’t to keep asking the same question over and over. Instead, we should state what we actually know. In many cases, that means acknowledging that we have multiple qualified suppliers, but we don’t know whether they share anything upstream.
That’s the reality, and it directly affects the viability of our “second source.”
How to Adjust for This Reality
The good news is that once we have faced this reality, the workflow stays the same. The qualification steps don’t need to be adjusted. Instead, a question needs to be added to them, and the answer needs to be something we can work with.
Start by asking yourself where your independence lives. Diversified vendors provide one level of independence. However, diversified process nodes, foundry relationships, assembly geography, and raw material paths deliver a much greater degree of autonomy.
The best approach in this situation is to ask yourself: is this a true alternative, or the same part in a different package? Once you have an answer to this question, the next step is to let the channel do the work you can’t do directly.
You may not know for certain if two parts are fabbed in the same place and in the same way, but you can use real-time intelligence to see if they behave as if they share the same constraints. Tracking the primary part and alternates together across authorized and independent distributors allows you to turn correlation into something observable over time.
If stock depth and lead times across every source for a part family tend to move in the same direction at the same moment, then you should treat that family as a single source until proven otherwise.
Is it a perfect approach? No, but few things are. It is, however, something you can do today, and an approach that provides far more protection than a generalized assumption based on supplier count.
A Few Final Takeaways
If we accept that a dual-sourced BOM is not a resilient BOM just by virtue of having more suppliers, then we can focus on the real work. Many organizations have adopted a supplier-count metric that’s easy to compute, but it has become increasingly disconnected from the thing it’s trying to track: real-time risk.
This worked for a time, but things have changed in recent years. It doesn’t mean that second sourcing is worthless; it simply means that we need to rethink how we approach it. Second sources can, and do, have shared dependencies that may rear their heads later on in the product lifecycle.
With access to real-time intelligence and part-level insights, teams can spot these dependencies and correlations with enough reliability to rethink their second-sourcing strategies before they become a larger issue.
So, next time you place a qualified alternate on your BOM, try checking lead times and availability across the entire part family with insights like those available on Findchips. You may find that there’s a deeper story hiding beneath the traditional “multiple suppliers” route.